Use Gstreamer playback 30Mbps streaming "H264_AVC_1080p_30fps_27Mbps_mp3.avi", while running iperf TCP streaming under the following two case:
1. Running the non-CBS kernel
2. Enable the FIQ kernel
Validate the Qav (Queue and Forwarding Protocol) which is developed by SW.
0001-GIC-FIQ-EPIT-implement.patch
0002-set-EPIT-priority-to-highest.patch
0003-GIC-support-SMP-4-cores-of-FIQ.patch
CBS &Shaper Patch:
0004-Implement-credit-base-shaper-alogrithim-to-schdule-A.patch
0005-enet-avb-CBS-SIRQ-rum-mode-pass-performance-stress-t.patch
Others Patch:
0006-Fix-the-61883-sub-type-protocol-check.patch
0007-Add-hrtimer-for-the-sirq.-Talker-transmit-packets-nu.patch
0008-1.-Fix-memory-map-size-issue.patch
0009-Increase-BD-entries-to-reduce-the-full-times.patch
0010-Add-sys-interface-to-log-out-the-video-packet-number.patch
0011-Add-AVB-timestamp-support.patch
0012-GIC-support-SMP-4-cores-of-FIQ.patch
Library: udp/output/libgstudp.so
Source: udp/*
1. Apply all the patches in the patch_whole.tar.gz in the attachment
2. Rebuild kernel 3.0.35:
Enable "CONFIG_ENET_IMX6_AVB" to support AVB.
Enable "CONFIG_RUN_IN_FIQ" in kernel: let CBS run in FIQ mode.
3. make uImage.
You can also use the uImage-avb-fig in the attachment directly. Flash to the SD card use dd command, the user gudie refer to the i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf.
Note: the uImage_org_nonavb in the attachment is the kernel image without QAV and FIQ.
Before the below action, you should already have seutp the Ubuntu Rootfs, copied all the Freescale *.deb files that come alone with the Release BSP demo image package and copied all the MM codec *.deb files (IMX_MMCODEC_3.0.7.tar) that from Freescale offical website, the user gudie refer to the i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf.
6. Know issues
If server A , Client B, client C and PC all are running ubuntu so on which machine we need to run avb kernel?
Second thing: is avb support available on 3.10 kernel?
How to git clone following
ssh://sw-git01-tx30.am.freescale.net/git/sw_git/repos/linux-2.6-testbuild.git
ssh://sw-git.freescale.net/git/sw_git/repos/Ethernet_AVB.git
Thanks
Thank you Xianfeng.
Hello Xianfeng Jin,
I have built 3.0.35_4.0.0 kernel with avb patches and it successfully boot with RUN_SIRQ configuration but does not boot with RUN_FIQ conf instead stops on requesting DHCP.
Thanks
On using image -- uImage-avb-fig, onto iMX6q Sabre for Automotive, the kernel hangs during boot up. So we applied patch_whole.tar.gz to linux kernel version 3.0.35_4.0.0 with RUN_FIQ conf. Ethernet is up and running, however dhcp request fails and no ip is obtained. When using RUN_SIRQ configuration ip is obtained and ethernet is working fine.
So we tried to use echo 1 > /sys/devices/platform/imx_wfi_issue.0/enable ; however there is no directory with name imx_wfi_issue.0 in our system.
Any help is appreciated!!!
Hi JinXianfeng,
Thank you for the response.
Currently I'm using imx6 Sabre Auto board with ubuntu 12.04.
All the patches are applied successfully as given above, and board-mx6q_sabreauto.c is also updated as in board-mx6q_sabresd.c. And hence i'm able to get the above issue solved. And now the network connection is established successfully. However, no data is being sent to the network from the server side on using gst-launch command . The logs are copied below. Please let me know if any more updates have to be done.
I'm using the following versions:
gst-plugins-good version: 0.10.31
firmware-imx-3.5.7-1.0.0
imx-lib-3.5.7-1.0.0
fsl-alsa-plugins-3.5.7-1.0.0
libfslcodec-3.5.7-1.0.0
libfslparser-3.5.7-1.0.0
libfslvpuwrap-3.5.7-1.0.0
gst-fsl-plugins-3.5.7-1.0.0
The multimedia codecs are built as given in the site:
http://boundarydevices.com/mx6-video-acceleration-raring-debian/
Log:
===
On monitoring the network data using wireshark, no data is send from server to the client. Please provide whether any updates have to be made.
In server side for the given command i'm getting the below log
==============
==============================================================================================
gst-launch-0.10 filesrc location=/usr/Sample.avi typefind=true ! aiurdemux name=d d. ! queue ! rtph264pay ! udpsink port=5000 host=192.168.2.255 sync=true d.! queue ! rtpmpapay ! udpsink port=5002 host=192.168.2.255 sync=true
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Aiur: 3.0.8
Core: AVI_PARSER_03.05.07 build on Jul 3 2013 01:47:35
mime: video/x-msvideo
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///usr/Sample.avi
Idx File:
/root/.aiur/.usr.Sample.avi.aidx
Seekable : Yes
Size(byte): 735524864
Movie Info:
Seekable : Yes
Live : No
Duration : 1:30:41.097984000
ReadMode : File
Track : 2
Track 00 [video_000000] Enabled
Duration: 1:30:41.097984000
Language: und
Mime:
video/x-divx, divxversion=(int)5, width=(int)660, height=(int)352, framerate=(fr
action)10000000/417083
Track 01 [audio_000000] Enabled
Duration: 1:30:40.992000000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int
)48000, bitrate=(int)0
^C Caught interrupt -- handling interrupt.
Interrupt: Stopping pipeline ...
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
[--->FINALIZE aiurdemux
====================================================================================================
In client side for the command given the below log is obtained
==============
====================================================================================================
gst-launch-0.10 udpsrc buffer-size=202400 do-timestamp=false uri=udp://192.168.2.255:5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264" ! rtph264depay ! queue ! vpudec low-latency=true ! mfw_v4lsink sync=false
MFW_GST_V4LSINK_PLUGIN 3.0.8 build on Feb 28 2014 05:45:17.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX6Q/D/S
vpudec versions : )
plugin: 3.0.8
wrapper: 1.0.38(VPUWRAPPER_ARM_LINUX Build on Feb 28 2014 05:20:01)
vpulib: 5.4.15
firmware: 2.3.10.40778
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
==================================================================================================
and in dmesg: No such IOCTL, cmd is 22032
=============
Thank you
Jithin
Hi Xianfeng Jin,
Could you please provide any feedback on this. We have tried applying the above patches and could not see any difference after applying the patch.
Could you please provide the uImage for sabre AI board with AVB enabled(uImage-avb-fiq for AI board)
Regards
Jithin
Hi Xianfeng,
Could you please suggest any links to download suitable h264 demo videos for testing AVB or can we get the link for file H264_AVC_1080p_30fps_27Mbps_mp3.av.
As per your suggestion we downloaded
from the below site
http://www.h264info.com/clips.html
the video
http://downloads.dvdloc8.com/trailers/divxdigest/300_rise_of_an_empire-trailer.zip
We could use pipe rtph264pay. However, it seems packets are not send from the server(we are using wireshark to monitor the Ethernet packets)
Are we missing something?
We are getting the below errors, and there is no data being send to the network.
command:
==========
gst-launch-0.10 filesrc location=/home/linaro/Documents/300.mp4 typefind=true ! aiurdemux name=d d. ! queue ! rtph264pay ! udpsink port=5000 host=192.168.2.255 sync=true d. -v --gst-debug=2
Errors
====
:aiurdemux_push_pad_buffer: Pad video push error type -4
0:00:00.315885667 5049 0x28150 WARN aiurdemux aiurdemux.c:3903
0:00:00.755606333 5252 0x28120 ERROR rtph264pay gstrtph264pay.c:560:gst_rtp_h264_pay_setcaps:<rtph264pay0> wrong avcC version
Also i would like to know if there are any kernel/debug prints to know if AVB is ON! Because we find same behaviour with both AVB and NonAVB kernel.
Could you please provide the uImage for sabre AI board with AVB enabled(uImage-avb-fiq for AI board)!! We have only AI board with us.
Any help is highly appreciated.
Regards
Jithin
Other customer and I have never seen such issue. But the demo image is used at MX6DQ_SabreSD board, so please refer to "i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide".
I suggest you don't apply these patch and make a clean version to build, ensure that your build steps are accurate.
Thank!
Hi Xianfeng,
Thank you for your support.
Now, I'm able to play the video in the client(there seems to be some issues with sending the audio).
But I could not make out any difference in performance with and without AVB Kernel.
Could you please let me know whether I can see any kernel prints to confirm that AVB is working as expected.
Attaching the logs for both NonAVB and AVB kernel.
Is it possible to provide an image for SABRE-AI board with the patch applied, just to verify that everything is working as expected.
Best Regards
Jithin
With NON AVB Kernel
====================
iperf gives
===========
[ 4] local 192.168.2.8 port 5001 connected with 192.168.2.3 port 48203
[ ID] Interval Transfer Bandwidth
[ 4] 0.0- 1.0 sec 11.2 MBytes 93.7 Mbits/sec
[ 4] 1.0- 2.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 2.0- 3.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 3.0- 4.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 4.0- 5.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 5.0- 6.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 6.0- 7.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 7.0- 8.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 8.0- 9.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 9.0-10.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 10.0-11.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 11.0-12.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 12.0-13.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 13.0-14.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 14.0-15.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 15.0-16.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 16.0-17.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 17.0-18.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 18.0-19.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 19.0-20.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 20.0-21.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 21.0-22.0 sec 10.8 MBytes 90.6 Mbits/sec
[ 4] 22.0-23.0 sec 10.3 MBytes 86.5 Mbits/sec
[ 4] 23.0-24.0 sec 10.3 MBytes 86.3 Mbits/sec
[ 4] 24.0-25.0 sec 10.5 MBytes 87.8 Mbits/sec
[ 4] 25.0-26.0 sec 10.4 MBytes 87.1 Mbits/sec
[ 4] 26.0-27.0 sec 10.6 MBytes 88.8 Mbits/sec
[ 4] 27.0-28.0 sec 10.4 MBytes 87.2 Mbits/sec
[ 4] 28.0-29.0 sec 10.4 MBytes 87.3 Mbits/sec
[ 4] 29.0-30.0 sec 10.3 MBytes 86.4 Mbits/sec
[ 4] 30.0-31.0 sec 10.5 MBytes 88.0 Mbits/sec
dmesg in client gives:
=======================
No such IOCTL, cmd is 22032
No such IOCTL, cmd is 22032
========================================================================
In the AVB kernel
=================
dmesg gives
===========
DVFS driver module loaded
mxc_WFI_ISSUE_probe, cpu = 2
add wake up source irq 88
WFI_ISSUE driver module loaded
No such IOCTL, cmd is 22032
No such IOCTL, cmd is 22032
iperf gives
===========
[ 4] 163.0-164.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 164.0-165.0 sec 11.2 MBytes 94.2 Mbits/sec
[ 4] 165.0-166.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 166.0-167.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 167.0-168.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 168.0-169.0 sec 11.2 MBytes 94.1 Mbits/sec
[ 4] 169.0-170.0 sec 10.6 MBytes 88.6 Mbits/sec
[ 4] 170.0-171.0 sec 10.3 MBytes 86.3 Mbits/sec
[ 4] 171.0-172.0 sec 10.3 MBytes 86.3 Mbits/sec
[ 4] 172.0-173.0 sec 10.5 MBytes 87.7 Mbits/sec
[ 4] 173.0-174.0 sec 10.5 MBytes 87.8 Mbits/sec
[ 4] 174.0-175.0 sec 10.6 MBytes 88.8 Mbits/sec
=======================================================================
End of Log
Best Regards
Jithin
Hi Jithin,
There have no kernel print to confirm AVB is working. I am wondering what’s video clip do you test, how much the bitstream? I suggest the bitstream of the video clip is as big as possible. I use 27Mbps video clip to test (H264_AVC_1080p_30fps_27Mbps_mp3.av).
I have no image for Sabre-AI board, I only have these image for Sabre-SD board for your reference.
FYI, I have sent a mail last week to you with attach image and same content as above, didn't you get it?
Hi All
i am quite new to LINUX.
I want to create automotive use-case using Ethernert-AVB for In-Vehicle-Infotainment,
by making use of i.mx6 SABRE for Automotive.
Example:
Two cameras 1)front-side view
2)Rear-side View
are connected to Head unit (i.mx6 SABRE Board)
could you please anybody suggest me which type of cameras should be used to get the Ethernet-AVB
form of data from camera and how to test the Ethernet AVB traffic on the network, as shown in
above example they made use of PC to test the Best-effort-lane, what is that exactly? Do i need to make
use of any AVB Supported switch in between cameras and Head unit(i.mx6 SABRE Board).
Any help is highly appreciated.
Hi Kajava,
Actually, I didn't test the AVB function using camera, I use the video clip to playback in server side and see and hear in client side. In order to demo the advantage of AVB, the server not only send audio and video stream, it also send best-effort etherent date to PC. For example, the current network bandwidth is 100Mbps, and no video to playback in server, the PC can receive the 80-90Mbps best effort data, when playback a 30Mbps stream video clip, the data throughoutput of the PC can be reduced to 60-70Mbps, the video can playback smoothly in client side at same time, it confirm the AVB function is working.
Normal switch is OK, don't need AVB support switch.
Thanks for your kind response,
Still i have some queries
1) What is meant by best effort Ethernet data, i didn't find any relevant information, Could you please elaborate something more on that?
2) what do you mean by " no video to playback in server"? is this mean there is another form of data other than Video.
3) Could you please elaborate more on distinguishing between the Ethernet Streaming and Ethernet-AVB streaming.
4) As you mentioned above we don't require any AVB supported switch, just because we, in our application currently using bandwidth of maximum 100Mbps?
what if we use greater bandwidth?
5) As per Ethernet AVB protocol, if we want to pass any AVB data through non-AVB switch cant be possible. do you have to say something on that?
6) how much feasible it is to Replaces the Server in Demo use-case with IP-Cameras?
Thanks
Anand
HI Anand,
Maybe my explanation confuse you, sorry, let me explain it again. From the above graphic, The talker(server A) provides the outgoing Audio Video streaming over the Ethernet. The listeners(Client B, Client C and Client Audio) receive Audio/Video streaming and play back/display. In the demo, all the devices are connected via a 100M TP-Link switch. Except for the AVB streaming, we will add extra Best-Effort traffic outgoing from talker to Notebook. The AVB streaming and Best-Effort traffic will compete for 100M bandwidth. The QAV is expected to guarantee higher priority for AVB streaming in TX queue.
Hi Xianfeng Jin,
Where do i get the Source code for AVB Stack used in above mentioned demon?
if avilable,Could you please share link?
Thanks
Anand
Hi Xianfeng
I am using i.mx6 Automotive SABRE board for development using LVDS display.
Following are the observations
1) File system mounts properly
2) shows promt after booting up the system
but
Unable to show anything on display (Display is Blank)..
Any help would be highly apperciated..
Following is the log for environemt variables
MX6Q SABREAUTO U-Boot > printenv
bootdelay=3
baudrate=115200
netmask=255.255.255.0
rd_loadaddr=(0x10800000 + 0x300000)
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
ethact=FEC0
serverip=192.168.149.158
bootfile=uImage
ipaddr=192.168.149.175
loadaddr=0x10800000
bootargs_base=setenv bootargs console=ttymxc3,115200
bootcmd=run bootcmd_mmc
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
stdin=serial
stdout=serial
stderr=serial
Environment size: 571/8188 bytes
Thanks & Regards
Anand Kajave
Hi Xianfeng Jin,
I am new to Linux And Ethernet AVB, presently we are using i.MX6 sabre AI board, our motto is to stream the video from Head unit and display it to RSE(Rear Seat Entertaiment). In this demo the procedure for shifting of Kernel with QAV and non AVB is not given. Please clarify the following doubts,
1) In BSP under which directory the patches should be placed to get U-Image?
2) In this you have given U-Image, whether this will support i.MX6 Sabre AI board?
3) If i load the kernel with the U-Image present in the SD card, how can i apply the patches?
PS: As am new to Ethernet AVB, please clarify these doubts.
Hi,
I able to stream video alone from i.MX6 sabre sd board to client PC by following below procedure:
On i.MX6 SDP target (as an example) :
$ ifconfig eth8 192.168.1.114
$ route add default gw 192.168.1.1 # local server
$ echo nameserver 8.8.8.8 >> /etc/resolv.conf # if I-net is needed
$ modprobe ov5642_camera
$ modprobe mxc_v4l2_capture
$ gst-launch mfw_v4lsrc capture-mode=4 ! vpuenc codec=12 ! tcpserversink host=192.168.1.113 port=5000
(My Linux PC host IP=192.168.1.113)
On Linux PC, under VLC, configure source as tcp://192.168.1.114:5000
I need video as well as audio streaming on Real time over Ethernet from i.MX6 Sabre Sd board to client host.
please help me to solve this issue.
Thanks,
Vidya
Hello Vidya Sagar,
From what I understand you need to implement AVB on the i.MX6. The PTP (IEEE 1588) driver is included in our Linux BSP but the rest of the AVB implementation needs to be implemented separately by software (as there is no HW module dedicated for AVB on the i.MX6) and it is there where this document comes in.
Have you tried the patches and steps on this document? If so, where in particular are you having problems?
See my comments:
1) In BSP under which directory the patches should be placed to get U-Image?
You can review the patch by Text Document, the head can guide you the patch code location.
2) In this you have given U-Image, whether this will support i.MX6 Sabre AI board?
No, it only works on the imx6DQ SabreSD board.
3) If i load the kernel with the U-Image present in the SD card, how can i apply the patches?
You should apply the patch to your BSP by git apply command, and then build the Uimage for AI board according to the User guide.
You can request to the link: https://community.freescale.com/message/346637#346637
I have applied the patch and it is successfully compiling. But when I enable the imx_wfi module using "echo 1 > /sys/devices/platform/imx_wfi_issue.0/enable" the system seems to be hung or crash. Is there any pad configurations required for EPIT to be enabled. Based on the code changes we require EPIT1_OUT to be configured which is either EIM_D19 or GPIO_0 or GPIO_7. Could you please tell whether the EPIT pads should be added in board_init ? Because in the BSP provided these pads are configured in different modes. Also please share the sabre-sd schematics if possible as i am not able to find the schematic in the site..
Hi jithin p,
I have the same issue with you when I run the command, gst-launch filesrc location=move.mp4 typefind=true ! aiurdemux name=d d. ! queue ! rtph264pay ! udpsink port=5000 host=10.193.102.255 sync=true d. -v --gst-debug=2
The log is :
......
......
Errors
====
:aiurdemux_push_pad_buffer: Pad video push error type -4
0:00:00.315885667 5049 0x28150 WARN aiurdemux aiurdemux.c:3903
0:00:00.755606333 5252 0x28120 ERROR rtph264pay gstrtph264pay.c:560:gst_rtp_h264_pay_setcaps:<rtph264pay0> wrong avcC version
......
How did you fix it ? Is it the problem of the video I play ?
Please help!Thanks.
Hi Xiafeng Jin,
Thanks a lot for the update. But can you tell the significance of using the sabre-sd hardware . Because according to the changes the platform with freescale IMX6Q processor should handle the changes. I am using the Freescale sabrelite version using IMX6Q processor which also uses the same FEC ethernet Controller. Could you please suggest why the imx_wfi module is not working in the sabre-lite version???
Thanks and Regards,
Mohamed Zubair.
Hi Xianfeng Jin,
We have a imx287 based customized board, Linux version using.2.6.35. To get exposure on AVB feature, We are planning to port your demo implementation on imx287 board. Currently the board has been used for automotive infotainment products.
Before that I have some basic questions Please can you clarify on the same.
1. To use your patches can i need to upgrade the linux version from 2.6.35 to 3.0.35?
2. Will I face any Hardware issues(MAC support in imx287)?
Thanks
Ashok
Hi Xianfeng
I am facing the same issue,
echo 1 > /sys/devices/platform/imx_wfi_issue.0/enable ; however there is no directory with name imx_wfi_issue.0 in our system.
do you have any patch for this issue. I am using same linux kernel version 3.0.35_4.0.0 and IMx6q sabre auto board.
Thank you
Hi Xianfeng
First of all I'm congratulating you, for your good work and patience to reply commenter's on this post. I'm also working in IMX6 family of processors.This demo is helpful for me to develop a avb-gst-plugin for my requirement. Currently I have one wand board dual and one sabre lite board.I need to send video/audio from sabrelite to wand board dual as avtp packets. I don't need to implement FIQ and AVB CBS (so I'm not applying the patches that you had attached already). I have doubts given in line.
1.The AVI video that you are sending have any specifications? Can I use my sample.avi?
2.Is this patch only for FIQ and AVB CBS? Or does it enable any hardware in your sabre-SD board?
3.Is this avb-gstreamer plugin can be usable for wandboard and sabrelite also? udpavbsrc and udpavbsink in the avb-gstreamer from your demo is only applicable for particular gst-launch commands shown in the demo? Or can I use this gst-avb-plugin with any other gst-launch command for sending mp3/wav/jpeg file as avtp and receiving this avtp packets(using udpavbsink and udpavbsrc respectively)?
This is what I did
1.Downloaded gst-plugins-good-0.10.31.tar.gz and your udp.tar.gz
2.Extracted both files and repcled udp in the gst-plugins-good-0.10.31 by udp given by you.
3.Compiled it for wand board dual and sabre lite
4.Then I run the sending command for avi file in sabre lite and receiving command for audio in wand board, but nothing find in wireshark for the AVTP packet.
Thanking You
Hello,
are there any plans to port this to gstreamer-1.0?
Best reagrds
Hello, I'm new of embedded Linux and are facing some trouble.
I'm working on iMX7D Sabre board, then
I would like know if it's possible runnig AVB demo implementation on this board.
Now, I'm trying to install a running Ubuntu distro on my iMX7D Sabre board as described in https://community.nxp.com/docs/DOC-328362 , but facing booting issues.
Any suggestions are very appreciated.
Thanks a lot
Best Regards