Setting i.MX8M Mini and Nano MIPI-DPHY Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting i.MX8M Mini and Nano MIPI-DPHY Clock

Setting i.MX8M Mini and Nano MIPI-DPHY Clock

The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.

  pastedImage_4.png

Calculating the video bandwidth

The video bandwidth is calculated with the following equation:

Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel

Taking as example the 1080p60 OLED display RM67191:

Pixels per second = 1920 x 1080 x 60 x 24

Pixels per second = 2985984000 = 2,98Gpixels/sec

Pixel clock calculation

The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file:

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

Line 530:

.pixelclock = { 66000000, 132000000, 132000000 },

Or the number can be obtained with the following equation:

pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate

pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60

pixel clock = 132000000 (rounded up)

Bit clock calculation (clock lane)

The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283):

sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

Bit clock can be calculated with the following equation:

bit_clk = Pixel clock * Bits per pixel / Number of lanes

In the case of 1980p60 (Raydium display), It is:

 

bit_clk = pixel clock * bits per pixel / number of lanes

bit_clk = 132000000 * 24 / 4

bit_clk = 792000000

Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file:

sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

評価なし
バージョン履歴
最終更新日:
‎12-20-2019 12:34 PM
更新者: