Build bootloader without spl in Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build bootloader without spl in Yocto

Build bootloader without spl in Yocto

Software environment: L5.4.47_2.2.0

Hardware i.MX8QXPC0 EVK board

In the uuu script we can see the bootloader imx-boot-imx8qxpc0mek-sd.bin-flash is necessary.

The default BSP build generate in the yocto project is with the spl, some customers are confused about the how to build the imx-boot-imx8qxpc0mek-sd.bin-flash.

Here I give the manually compile way and generate it in yocto.

In the yocto generate it is more convenient than the manually compile way.

Hope this can do help for you.

附件
无评分
版本历史
最后更新:
‎06-17-2021 02:30 AM
更新人: