Android N7.1.2_2.0.0 GA Release Announcement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android N7.1.2_2.0.0 GA Release Announcement

Android N7.1.2_2.0.0 GA Release Announcement

The i.MX Android N7.1.2_2.0.0 GA release is now available on IMX_SW page.

 

  • Files available:

#

Name

Description

1

android_N7.1.2_2.0.0_docs.tar.gz

i.MX Android N7.1.2_2.0.0 BSP Documentation

2

android_N7.1.2_2.0.0_source.tar.gz

Source Code of Android N7.1.2_2.0.0 BSP (4.1 kernel) for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite, i.MX6SX and i.MX7D

3

android_N7.1.2_2.0.0_image_6dqpsabreauto.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite

4

android_N7.1.2_2.0.0_image_6dqpsabresd.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite.

5

android_N7.1.2_2.0.0_image_6slevk.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - i.MX 6Sololite evaluation kit.

6

android_N7.1.2_2.0.0_image_6sxsabresd.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 6SoloX

7

android_N7.1.2_2.0.0_image_6sxsabreauto.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX

8

android_N7.1.2_2.0.0_image_7dsabresd.tar.gz

Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 7Dual

9

fsl_aacp_dec.tar.gz

AAC Plus Codec for N7.1.2_2.0.0

10

android_N7.1.2_2.0.0_tools.tar.gz

Manufacturing Toolkit and VivanteVTK for N7.1.2_2.0.0

 

  • Supported Hardware SoC/Boards:
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform
    • i.MX 6SoloLite EVK platform
    • i.MX 6SoloX SABRE-SD board and platforms
    • i.MX 6SoloX SABRE-AI board and platforms
    • i.MX 7Dual SABRE-SD board and platform

 

  • Changes:

Compared to the N7.1.1_1.0.0 release, this release has the following major changes:

    • Upgraded the Android code base from android-7.1.1_r13 to android-7.1.2_r9.
    • Upgraded U-Boot from v2015.04 to v2017.03.
    • Upgraded the kernel from v4.1.15 to v4.9.17.
    • Upgraded the GPU driver from 6.2.0.p2 to 6.2.2.p1.
    • Upgraded the Wi-Fi BCMDHD release version to 1.141.100.6.
    • Refine the Gralloc and HWC HAL.
    • Enable the GPT partition to replace the MBR partition.

 

  • Feature:

For features please consult the release notes.

 

  • Known issues

For known issues and more details please consult the Release Notes.

评论

the mfgtool is null.can not bu use.

Hello,

  N7.1.2. MFG tool package on the Web is empty.
Please look at "Android_Quick_Start_Guide.pdf", in particular at section 3.3 (Flashing
board images) how to use files from OS (demo) images, that may be found on the Web.

Regards,

Yuri.

I know .But android_N7.1.2_2.0.0_tools\mfgtools\Profiles\   this dir is empty,  all have nothing.

you can download the mfgtools from the web ,and try.

thanks

android_N7.1.2_2.0.0_tools\mfgtools\Profiles\ this dir is empty. you can download the mfgtools from the web ,and try.

Wilson.chen

我的企业

mfgtools can not open

You may try mfg of the previous release (N7.1.1) and change target image files (from N7.1.2) 

~Yuri.

nxp,

          anybody knows?

          the mfgtools  can not work,  

Miss AAC Plus Codec for N7.1.2_2.0.0 files.

the link will show the below error message!
can’t find the file at https://cache.nxp.com/secured/bsps/fsl_aacp_dec.tar.gz?__gda__=1514195832_11c95d7af3cee83ac21ceaf2c6....

I have the same problem. Is there any alternate mirror or link to the correct uri?

The link for IMX_N7.1.2_2.0.0_AACPlus is invalid

Hello AckeyCheng

We hope to get AACPlus codec, but Link problem has not been solved for a long time.

Do you have a plan to fix this problem?

Best regards,

Ishii.

无评分
版本历史
最后更新:
‎10-20-2017 01:24 AM
更新人: