141-00207-509C_iMX6X_SX-SDCAN_QSG.pdf

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

141-00207-509C_iMX6X_SX-SDCAN_QSG.pdf

141-00207-509C_iMX6X_SX-SDCAN_QSG.pdf

Application Note covering how to get the Silex SX-SDCAN working with the Sabre-SD i.MX6 Evaluation kit.

附件
评论

This app note may be a bit outdated.  We are now at SDK L3.0.35_4.1.0.

Myself and another FAE are unable to get this card to be recognized in a standard Linux LTIB build.

When I insmod the driver, I get errors.

Also, I contacted Silex for the calData_SX-SDMAN.bin file but have not received it.

Can you offer any updates to the app note so I can get this card to be recognized?

Bradley,

We are actually releasing a new EVK for the Silex SX-SDCAN for the Sabre-SD board. Same radio hardware with an SD card that includes a bootable Ubuntu image with our latest driver, supplicant and wireless tools. I should be able to get you a copy of the image sometime next week if you're interested. It has an updated users Manual and QSG.

...Andy

Please any one can provide the Latest SX-SDCAN Application Note or Procedure to test in Linux for Freescale Yocto Latest release Version 1.6 Daisy. It uses linux-3.10.53 Kernel.

Regards,

Dooty.

Dooty,

We have actually ported to the linux-3.10.17 Yocto kernel and are in the process of porting to the latest linux-3.10.53. However it will be a few weeks before we will have the supporting application note available.

If you contact me directly at aross@silextechnology.com we can go through the information I have immediately available.

Regards....Andy

无评分
版本历史
最后更新:
‎04-18-2013 01:11 PM
更新人: