about long-term wireless stability of the QN9080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about long-term wireless stability of the QN9080

Jump to solution
3,892 Views
jung-jin
Contributor II

Hello

Our product is using QN9080.
It disconnects well between 5 and 15 minutes after Bluetooth connection.
The wireless environment is at the level of a general office and is not noisy.
The goal is to operate stably for more than 8 hours.
The transmission interval is 40 ms, and the communication speed is around 30 kbps.
What variables can be adjusted to increase wireless connection stability?

ex)
(1) Increase memory or queue size?
- gMaxL2caQueueSize_c ?
- gPrepareWriteQueueSize_c ?

(2) Increase timeout or some time parameter?
- gBleDefaultTxTime_c?
- connection interval or latency?

(3) or user coded phy?


Please let me know if there is a way to increase the stability of wireless connection by adjusting certain parameters.

Best Regards,
jung jin

Labels (2)
0 Kudos
Reply
1 Solution
3,501 Views
jung-jin
Contributor II

Finally, it was confirmed that reboot occurs randomly due to i2C communication
Decreasing I2C speed from 400 kHz to 100 kHz resolved the issue
I don't know why it reboots sometimes when I set I2C to 400 kHz.


Thank you for your reply.

View solution in original post

0 Kudos
Reply
8 Replies
3,844 Views
acklyn
Contributor I
QN9080 integrates a 32-bit ARM Cortex-M4F core with Bluetooth Low Energy (v5.0)
compliant radio, link controller, host stack and GATT profiles. The 32-bit ARM Cortex-M4F
MCU and on-chip  memory provides additional signal processing and scope to run scentsy workstation
applications for a true single-chip Bluetooth Low Energy (v5.0) solution.
0 Kudos
Reply
3,872 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi jung jin,

 

Hope you are doing well. How are you connecting the QN9080? (Other device or to another QN9080).

What SDK example are you using as a base? What modifications did you make?

Are you using the QN9080DK board? Or is it a custom board?

 

Best Regards,

Ricardo

0 Kudos
Reply
3,867 Views
jung-jin
Contributor II

Hi Ricardo.

(1) QN9080 device - Smart phone (android)
(2) Our project based on private_profile_client
- Bluetooth-related functions have not been modified, but only application-related functions.
(3) Our custom board

<more information>
- Bluetooth connection is sometimes disconnected between 10 and 15 minutes.
- Sometimes, it's stable for more than an hour.
- Sometimes the device reboots when the connection is disconnected.

If there's a way to improve the stability of wireless communication, I hope you can let me know.

Best Regards,
jung-jin

0 Kudos
Reply
3,831 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi jung-jin,

 

Are you having this issue with the private_profile_client without any modification? Have you try with two QN9080 boards? We don't know if the disconnection is caused by the QN9080 or by the android application.

By any chance, could you print the disconnection reason?

In the gConnEvtDisconnected_c case of the BleApp_ConnectionCallback, please add these lines:

Serial_Print(gAppSerMgrIf, "Disconnection Reason:  ", gNoBlock_d);

Serial_PrintDec(gAppSerMgrIf, pConnectionEvent->eventData.disconnectedEvent.reason);

Serial_Print(gAppSerMgrIf, ".\n\r", gNoBlock_d);

 

What is the Disconnection Reason?

 

Regards,

Ricardo

0 Kudos
Reply
3,816 Views
jung-jin
Contributor II

Hi Ricardo.

When I tested with the proposed code, the disconnection message was not printed.
When I checked, it was not a Bluetooth disconnection problem, and a sudden reboot occurred during operation.
I'm not sure why the device suddenly reboots randomly during Bluetooth communication.

Is there any way to print out a message to find out the cause of the reboot?
Our company's three products developed by applying QN9080 seem to show similar trends.
- It operates for as short as 5 minutes, as long as 1 hour, and then suddenly reboots.
- Bluetooth connection will be disconnected when rebooting.

Best Regards,
jung-jin

0 Kudos
Reply
3,781 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi jung-jin,

 

Can you please check this register?

(From the User Manual)

Ricardo_Zamora_0-1646674807880.png

 

This could help us to identify the issue you are presenting.

Do you have a QN9080DK? Is this issue also happening in our board? This to discard an issue with your custom board.

 

Regards,

Ricardo

3,502 Views
jung-jin
Contributor II

Finally, it was confirmed that reboot occurs randomly due to i2C communication
Decreasing I2C speed from 400 kHz to 100 kHz resolved the issue
I don't know why it reboots sometimes when I set I2C to 400 kHz.


Thank you for your reply.

0 Kudos
Reply
3,734 Views
jung-jin
Contributor II

Hi Ricardo.

Currently, I am reading the reset source register after initializing uart.
Is it right to read it as below?

Serial_Print(gAppSerMgrIf, "RST_CAUSE_SRC : %x", SYSCON->RST_CAUSE_SRC & SYSCON_RST_CAUSE_SRC_RESET_CAUSE_MASK, gAllowToBlock_d);

The register value read after a sudden reboot occurs is 0x1FF.
Does this mean that power on reset has occurred?

+ more info

 - Rebooting occurs even when Bluetooth is not connected. (Waiting with only advertising)
 - When it's okay, it works normally for more than 5 hours.
 - Sometimes the QN9080 board reboots in five minutes.

Regards,

Jing-jin

0 Kudos
Reply