MTBF Data for BGA3023Y

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MTBF Data for BGA3023Y

2,156件の閲覧回数
harshithram
Contributor II

Hi,

We are using BGA3023Y-1.2GHz 20dB Gain CATV Amplifier in our design. What is the MTBF/Failure rate of that device?

Regards,

Harshith

2 返答(返信)

2,068件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

The BGA3023 is no longer manufacturer and the MTBF is no longer available, all the information about this part is obsolete

BGA3023 Product Information|NXP 

Regards

2,068件の閲覧回数
harshithram
Contributor II

Thanks Vicente !

--

Regards,

Harshith

From: vicentegomez <admin@community.nxp.com>

Sent: Wednesday, May 13, 2020 3:49 AM

To: Harshithram KV <harshithram@saankhyalabs.com>

Subject: Re: - Re: MTBF Data for BGA3023Y

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MTBF Data for BGA3023Y

reply from Vicente Gomez Salazar

<https://community.nxp.com/people/vicentegomez?et=watches.email.thread>

in *Wireless

Connectivity* - View the full discussion

<https://community.nxp.com/message/1310884?commentID=1310884&et=watches.email.thread#comment-1310884>

0 件の賞賛
返信