HAN Communication Error (ZPS Error received 4)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAN Communication Error (ZPS Error received 4)

1,933件の閲覧回数
vihang_jani
Contributor I

Test Scenarios :
- I have two devices, which are joined with Communication Hub.
- One of them is Electric meter(Type1) Device and another one is Prepayment Device(Type2).
- Both are having same APS key for HAN communication between them.

Problems :

- Whenever Type2 device send data to Type1 device in HAN Network, Type1 device is getting ZPS Error received 4.

- I have performed same scenarios in Sprint11(NXP SDK - JN-SW-4170-v1758) as well in Sprint12(NXP SDK - JN-SW-4170-v1773).
- In Sprint11 Type1 device can able to receive data which are sent from Type2 device.
- In Sprint12 Type2 device not able to receive data which are sent from Type2 device, as Type1 device is getting ZPS Error received 4.

ラベル(1)
0 件の賞賛
返信
1 返信

1,801件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vihang,

Could you please provide more information about your issue?

 

Are you working on JN-SW-4170 v1758? We do not have that version, we only provide 1745.

Could you please confirm this?

 

Did you take as a reference some example?

Anyway, it will be very useful if you can take a screen about this issue.

Mario

0 件の賞賛
返信