End device with automatic wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

End device with automatic wake up

2,988件の閲覧回数
raheleh
Contributor II

Which one of the zigbee demo applications from beekit demonstrates an end device that automatically wakes up from Doze or Hibernate based on internal timeouts or clock ticks?

we have an end device with scheduled automatic wake up but it misses the wake up every once in a while. 

Thanks!

0 件の賞賛
返信
2 返答(返信)

2,792件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Raheleh,

As you know the beekit is the old version for the zigbee stack. 

Could you please take a look for the Beestack 5.0.0?

https://www.nxp.com/webapp/Download?colCode=KINETIS-BEESTACK&appType=license&location=null&fsrch=1&s... 

Hope it helps

Let me know if you have problems with the examples

Mario

0 件の賞賛
返信

2,792件の閲覧回数
raheleh
Contributor II

Hi Mario, 

we have to troubleshoot this problem for our existing MC13226 based devices.

so i don`t think referring to the kinetis series helps. 

there must be examples on the old beekit as well for sleepy devices. let me know please if you are aware of them. 

thanks!

0 件の賞賛
返信