Enable security MQTT client for RW612

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable security MQTT client for RW612

242 Views
TrevorHsu
Contributor I

Hi 

We tried importing the SDK example "wifi_mqtt" and found the "mqtt_client_info" structure, it doesn't seem to enable the security in the default example, please see the following screenshot.

Referring to the sample code, it needs enable the "LWIP_ALTCP " & "LWIP_ALTCP_TLS" macros to enable security. Do you know how to enable security? or do you have a guide for opening "LWIP_ALTCP " & "LWIP_ALTCP_TLS" macros using the wifi_mqtt example?

 

 

 

 

ddddddd.png

BR

Trevor

 

0 Kudos
Reply
3 Replies

156 Views
TrevorHsu
Contributor I

Hello, 

Regardiing the above example, it seems that the Lwip MQTT function library is not used(replace with the coreMQTT library).

Could you help check if RW61x support secure MQTT with Lwip library?

0 Kudos
Reply

89 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

I check internally about this, and I'm afraid that we currently do not have an example with those features enabled . In this case there are some macros that can be enabled still,  it will be up to every customer to adapt the examples and add the features.

 

I apologize for the inconvenience

 

Regards

0 Kudos
Reply

202 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

 

Could you please help me check the frdmrw612_aws_shadow_wifi_nxp example? After checking the different examples available this would be the closest example that we have for the request. 

Could you please help me check and validate it this works for you? 
 
Regards, 
 
0 Kudos
Reply