88W8997+ Non-NXP platform / BT logo certification and BT Host QDID question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

88W8997+ Non-NXP platform / BT logo certification and BT Host QDID question

739件の閲覧回数
yao_feng
Contributor III

Product info: Non - NXP platform + 88W8997 AZW AW-CM276NF module.

Customer is going to do BT logo certification and they have below question:

1. Will NXP share your BLUEZ code base or BT Host QDID to customer?
2. or when the product which is using NXP WiFi-BT combo chip but non-NXP platform; this case uses 88W8997 module + Sigmastar platform/main CPU.
can customer directly use the NXP HOST QDID: https://device.report/bluetooth/129162

Thanks.

= = =

Customer's note below:

  1. NXP是否會提供其NXP 所使用的BLUEZ code base or BT Host QDID
  2. 或是當Product design 所搭配的是NXP BT CHIP, 就可以直接以AVNET所提供的這組QDID來宣告&Reference

        - "https://device.report/bluetooth/129162 | Declaration ID: D052927 (52927)"

ラベル(2)
0 件の賞賛
返信
1 返信

684件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Customers can qualify their end products by combining different qualification listing QDIDs together, still, please consider that while there is a pre-certification they will still need to certify their end application as there are differences in the hardware and there might be some modifications in sw configuration that might affect the performance.

 

regards,

0 件の賞賛
返信