Has anyone had any success in getting multiple controllers based on AN-1171 to connect via LightLink. I can connect to multiple lighting devices fine, but I cannot get 2 controller to connect (the second one is factory new).
As per the instructions I am pressing the button to start the commissioning simultaneously on both (or as simultaneously as I can humanly achieve), but looking at the debug information, neither seem to see the requests from the other.
Ok, further investigation says I am receiving the interpan data on the second (factory new) unit.
From the serial debug
ZCL_Task got event 22
& event 22 by definition is ZPS_EVENT_APS_INTERPAN_DATA_INDICATION
but nothing further happens, it appears to be thrown away in vZCL_HandleInterPanIndication