* Test environment :
- JN5169
- SDK : JN-SW-4168
- device : Coordinator, Router, Sleepy device
- JN-AN-1189 & JN-AN-1184
When The sleepy device be joined through the router, the following message was outputted in coordinator.
ERROR: Extended status 0x87
ERROR: Extended status 0x87
APP: vCheckStackEvent: ZPS_EVENT_AF_DATA_INDICATION <- this is zcl basic report message of sleepy device.
In zps_nwk_pub.h, ZPS_teExtendedStatus 0x87 is the following.
// 0x87 There are no free entries in the extended address table. The extended address table is configured in the config editor
What is that problem?
Additionally I want to know following.
At this time, there is no information about join in the coordinator.
I wants to the coordinator knows the information that the sleepy device be joined through the router.
Best Regards.
Hi, Xiao
Can you post your configuration in AN1223 zpscfg file together with that of mainspoweroutlet in its zspcfg file ?
for example, if you want to set up nwk with 100 mainspoweroutlet , you can set followings in AN1223 zpscfg file:
1) Mac Table Size = 100
2) Active Neighbour Table Size + Address Map Table Size = 100 ( suggest that keep Active Neighbour table size as default value 26 in case no fragmentation for link status message, then Address Map Table Size can be set to 100-26=74)
3) Routing Table Size can be set to same value (74) as that of Address Map Table Size.
Hi Lee,
Please set up the Default Extended PAN id different from 0. Zigbee Pro Editor.
I want to the coordinator knows the information that the sleepy device be joined through the router.
The coordinator is receiving a device announce from the router.
Look for the case ZPS_EVENT_NWK_JOINED_AS_ROUTER:
case ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE:
API vHandleStackEvent on the app_coordinator.c
Regards,
Mario
Hi Mario,
I have tested to Default Extended PAN Id 0x0000000000000001.
But that result is also error.
ERROR: Extended status 0x87
ERROR: Extended status 0x87
Also the coordinator not receives ZPS_EVENT_NWK_JOINED_AS_ROUTER or ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE.
And, Why not set to the Default Extended PAN Id is zero?
Best Regards,
Lee
Hi Mario,
I am ready for long time.
Is this bug?
Best Regards,
Lee
Hi Lee Wonsoo,
Did you capture all the packets in the air? Could you please provide this sniffer log?
Regards,
Mario
Hi Lee,
I had checked the sleep device that you are using and works fine.
Could you please confirm the example that you are using? I will try to replicate the issue and I need the same scenario.
Coordinator: JN-AN-1189 or JN-AN-1184?
Router: JN-AN-1189 or JN-AN-1184? DimmableLight? ColorDimmableLight?
Sleep End device, I used the JN-AN-1184, but I defined the ZPS_vAplSecSetInitialSecurityState that is not included.
Regards,
Mario
Hi Mario,
Coordinator: JN-AN-1189, Coordinator
Router: AN1184_ZBP_Router
Sleep End device: JN-AN-1189, OccupancySensor
I defined the ZPS_vAplSecSetInitialSecurityState that is included.
PUBLIC uint8 s_au8LnkKeyArray[16] = {0x5a, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6c,
0x6c, 0x69, 0x61, 0x6e, 0x63, 0x65, 0x30, 0x39};
ZPS_vAplSecSetInitialSecurityState(ZPS_ZDO_PRECONFIGURED_LINK_KEY, (uint8 *)&s_au8LnkKeyArray, 0x00, ZPS_APS_GLOBAL_LINK_KEY);
Regards,
Lee
Hi Mario,
How's it going?
Regards,
Lee
Hi Lee Wonsoo,
Could you please provide the set up that you have on the coordinator? Advance properties on the zpscfg file.
Regards,
Mario
Hi Mario,
Advance properties is the following.
Regards,
lee
Hi Lee,
What is the version that you have SDK and AN?
Did you modify the code?
Regards,
Regards,
Hi Mario,
I also encountered an error with ERROR: Extended status 0x87, because I connected more than 100 devices, this error will appear.
the following is the advanced parameter configuration of my coordinator in the zpscfg file
This problem has been bothering me for a long time, please help me
Regards,
Daniel
Hi Daniel,
I have the same situation as you, 0x87 and 0x85, have you solved it?
I added about 40 ZR and 20 ZED