UWB - MK UWB Mobile Edition Evaluation Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UWB - MK UWB Mobile Edition Evaluation Kit

1,299 Views
patsn
Contributor I

With this module, I understand that I can use an iPhone and its U1 chip.

I have some questions :

- Is the kit is compatible with an Samsung S21 Ultra phone which has an embedded UWB chip ?

- Can I add a NFC shield to the arduino equiped with the UWB Tag SR040 ? The purpose is to exchange data between the arduino through NFC protocol when the arduino is close to an mobile phone. Is this possible to do so ? My project is to open through a small distance (50cm) calculated by UWB a door equiped with a NFC reader. I approach the door (50cm) my phone send data through Bluetooth for example, and the reader take the data sent and then open the door.

 

Is it a feasible project ?

0 Kudos
Reply
1 Reply

1,271 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Could you please redirect your question to Mobile Knowledge?

They will be able to help you with the support of their kit.

 

Best Regards,

Ricardo

0 Kudos
Reply