Replace with the same type function, an error happen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replace with the same type function, an error happen

968 Views
964884134
Contributor I

As we see in the picture: when I try to change the function "....AsInitiator" and rebuilt the projet , an error happen .These two functions ,"....AsInitiator" and "....AsTarget" , should be the same type and on the same header file, why is there an error that can't find the object? Undefined Symbol ?

Tags (1)
0 Kudos
Reply
1 Reply

882 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please share with me the release version of the SDK you are using? I just downloaded the latest one and the latest AN1217, just changed that line just as you have it and everything builds correctly.

target build.png


Did you modify something else?

Regards, 

Estephania 

0 Kudos
Reply