Where can I find the latest firmware version for the QN9080 dongle? Apparently it should appear in the QTool installation directory, but I can not find it. I'm using the QTool Rev. 1.0.0, released on 2018-02-01.
Solved! Go to Solution.
Hi,
The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup
To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive.
-Anthony
Hi,
The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup
To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive.
-Anthony
Hi Borja,
The QTool software is being updated very soon to include the firmware. I'll post back when the new version is available.
-Anthony