PN7642 SPIA master mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7642 SPIA master mode

Jump to solution
459 Views
artem_pn
Contributor II

Hello! 

I am using PN7642. I would like to ask is it possible to use SPI that is connected to host interface pins ATX_A, ATX_B, ATX_C, ATX_D in master mode or it can be configured only to work in slave mode? 

Thanks in advance! 

Artem

 

0 Kudos
Reply
1 Solution
430 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @artem_pn

Hope you are doing well.

Host Interface pins may be intended for SPI target functionality. SPI controller should have dedicated pins according to PN7642 Data Sheet, Section 8 pinning information.

Regards,
Eduardo.

View solution in original post

0 Kudos
Reply
2 Replies
431 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @artem_pn

Hope you are doing well.

Host Interface pins may be intended for SPI target functionality. SPI controller should have dedicated pins according to PN7642 Data Sheet, Section 8 pinning information.

Regards,
Eduardo.

0 Kudos
Reply
409 Views
artem_pn
Contributor II

Thank you!

0 Kudos
Reply