'Nothing to build' error with PN762C example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'Nothing to build' error with PN762C example

Jump to solution
1,650 Views
Pel
Contributor III

Hello NXP team,

 

I'm trying to program the PNEV7462C with some example project from the PN7462AU FW and SW Examples Full Version - v06.10.00 zip file (SW3683.zip). When I try to guild a project MCUxpresso give me the following error:

----

**** Build of configuration DebugPN7462AU for project PN7462AU_ex_phExVCom_mcux ****

Nothing to build for project PN7462AU_ex_phExVCom_mcux

----

I downloaded and uploaded the SDK from the FRDM-K82F board in the 'Installed SDKs' window (SW3827.zip : SDK_2.x_FRDM-K82F). I imported the example with the 'Import project(s) from file system...' function from the Quickstart menu and pointed it to the SW3683.zip file. When I imported it only the mucx extension (<project name>_mcux) project appeared and when I tried to build it the discussed error popped-up.

 

Can you help me find out what have I done wrong ?

Best regards,

Alexandre Pellerin.

0 Kudos
Reply
1 Solution
1,615 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>>Is the PNEC7462C board compatible with the FRDM-K82F SDKs and its example ?

Because some examples have the MCU setting. Like NFC Forum . SDK for Freedom K82 Board ([http://www.nxp.com/products/:FRDM-K82F]). The
pre-build SDK can be downloaded from
[https://mcuxpresso.nxp.com/en/license?hash=9897a8c19a6bc569c3fade7141f0f405&hash_download=true&to_va...]
See MCUXpresso User Manual for steps needed to install an SDK.

 

>> Also how can I import the example from the 'PN7462AU FW and SW Examples Full Version - v06.10.00.zip' ? When I import them, they are empty _mcux projects.

Please kindly refer to the thread for the more information.

URL:https://community.nxp.com/t5/Other-NXP-Products/PN7462-SW3683-no-source/td-p/1363362

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
3 Replies
1,644 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please download SDK of K82 as the link.

URL:https://mcuxpresso.nxp.com/en/select.

And 'Installed SDKs' window in MCUXpresso.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

0 Kudos
Reply
1,635 Views
Pel
Contributor III

Hello Fangfang,

 

Is the PNEC7462C board compatible with the FRDM-K82F SDKs and its example ?

Also how can I import the example from the 'PN7462AU FW and SW Examples Full Version - v06.10.00.zip' ? When I import them, they are empty _mcux projects.

 

Have a nice day,

Alexandre Pellerin.

0 Kudos
Reply
1,616 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>>Is the PNEC7462C board compatible with the FRDM-K82F SDKs and its example ?

Because some examples have the MCU setting. Like NFC Forum . SDK for Freedom K82 Board ([http://www.nxp.com/products/:FRDM-K82F]). The
pre-build SDK can be downloaded from
[https://mcuxpresso.nxp.com/en/license?hash=9897a8c19a6bc569c3fade7141f0f405&hash_download=true&to_va...]
See MCUXpresso User Manual for steps needed to install an SDK.

 

>> Also how can I import the example from the 'PN7462AU FW and SW Examples Full Version - v06.10.00.zip' ? When I import them, they are empty _mcux projects.

Please kindly refer to the thread for the more information.

URL:https://community.nxp.com/t5/Other-NXP-Products/PN7462-SW3683-no-source/td-p/1363362

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply