Hi to all,
Hope you all are doing good in this tuff time.
We are working on a project based on mkw41z512 with the BLE stack.
We were adding the "over the air firmware programming" feature in our project for which we are using the NXP toolbox application.
We are planning to build our own android application for which we require the source code of the IoT Toolbox application.
It would be a great help if anyone from NXP can provide us the source code.
Thanks in advance for your precious time.
Hi,
Unfortunately, the code is not open source.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thanks for your reply.
Can we have any software flow diagram or such kind of documents related to the android which can help us building the OTAP server on the android application?
Any help will be appreciated.
Hi,
In directory 'SDK_2.2.2_FRDM-KW36 - MCUXpresso\docs\wireless\Bluetooth\Bluetooth Low Energy Application Developer Guide.pdf', it describe the otap in detail.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------