In MKW24D512V, can I use pin 6 (SPI0_SOUT), pin 7 (SPI0_SIN) and pin 8 (SPI0_SCK) to create an SPI interface or have to use pin 5 instead of pin 8.
Hello Vassil,
There should not be any issue when using PIN 8 instead of PIN 5 for SPI0_SCK signal. Please just make sure you properly set the registers and pin functionality. You may use any of our code examples included in BeeKit as reference. Let me know if you have any issues.
Regards,
AngelC