I'm experimenting with the Heart Rate Sensor sample project (KDS, bare metal OS) on the USB-KW41Z board.
When I enable the low power feature however, I don't get the expected advertising. (And the SWD connection dies, which is expected) The only real code changes are setting these flags in the preinclude file:
#define cPWR_BLE_LL_Enable 1 #define cPWR_UsePowerDownMode 1 #define gTMR_EnableLowPowerTimers 1 #define cPWR_CheckLowPowerTimers 1
If I modify the project to start advertising immediately, I get advertisements for a second or two then nothing.
Is the BLE deep sleep feature known to work with this sample? Is there more configuration required? Any suggestions or advice appreciated.
NOTE: I've gotten past this particular symptom, but still seeing other issues with advertising while BLE_LL deep sleep is enabled. Will be updating later.
Hey Richard,
Any updates?
Thanks,
Evgeny