Here is my configuration:
app_preinclude.h:
#define gAppUseNvm_d 1
...
#if gAppUseNvm_d
/* configure NVM module */
#define gNvStorageIncluded_d (1)
#define gNvFragmentation_Enabled_d (1)
#define gNvUseFlexNVM_d (1)
#if gNvUseFlexNVM_d
#define gUnmirroredFeatureSet_d (0)
#else
#define gUnmirroredFeatureSet_d (1)
#endif
#define gNvRecordsCopiedBufferSize_c (128)
#endif
NV_Flash.c:
#define gEEPROM_DATA_SET_SIZE_CODE_c (0x33U)
//#define gEEPROM_DATA_SET_SIZE_CODE_c (0x39U)
/*
* Name: gFLEXNVM_PARTITION_CODE_c
* Description: FlexNVM partition code
*/
#define gFLEXNVM_PARTITION_CODE_c (0x3U)
memory:
sdk:
When I enable battert level notification, Gap_CheckNotificationStatus returns gDevDbCccdNotFound_c, so it can not send notifications.
handleCccd is 27, I can found it in static_gattDatabase:
if I set gAppUseNvm_d to 0, Gap_CheckNotificationStatus returns 0.
Hi,
Hope you are doing well. First of all, I would recommend to check your memory Locations and Sizes. For this you can refer to section 4.6.1.1 of the Reference Manual (pages 135-138).
We have made the following test:
First, using the flexnvm example, with gEEPROM_DATA_SET_SIZE_CODE_c (0x33U) and gFLEXNVM_PARTITION_CODE_c (0x3U).
And then, running the HRS example, with the following memory configuration:
And we were able to get the Notification Status correctly:
So you need to check your memory settings and also I would recommend to use the newest SDK version.
Regards,
Ricardo
Hi, Ricardo
Thank you very much for your reply! Now after I initialize eeprom, I don't use it and no problem occurs. But if I write data to the eeprom (starting from 0x14000000), I get this problem. I see that SDK seems to use NVM_RegisterDataSet to save cccd data, I wonder if it will conflict with my eeprom use here?