JN5168 - Synchronize Between 2 devices (router-router/router-end device)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5168 - Synchronize Between 2 devices (router-router/router-end device)

589 次查看
fehnrirx
Contributor I

I need to know how to synchronize between 2 devices, light switch for example, where when i turn switch 1, it also turn on the switch 2, and so on. or at least the main switch will change it state whether the secondary switch is used. the purpose is like 2-way switch, where i can control the light with these switch. my base code is using JN-AN-1189. thanks

标记 (2)
0 项奖励
回复
1 回复

414 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi William,

If a controller node is bound to one or more light nodes The lights will be controlled synchronously.

I recommend you take a look at the JN-AN-1189-ZigBee-HA-Demo-1v15.pdf

Chapter: 6.2.2 Commissioning Light Nodes - Binding

Please follow the next path.C:\NXP\bstudio_nxp\workspace\JN-AN-1189-ZigBee-HA-Demo\Doc

Regards,

Mario

0 项奖励
回复