I need to know how to synchronize between 2 devices, light switch for example, where when i turn switch 1, it also turn on the switch 2, and so on. or at least the main switch will change it state whether the secondary switch is used. the purpose is like 2-way switch, where i can control the light with these switch. my base code is using JN-AN-1189. thanks
Hi William,
If a controller node is bound to one or more light nodes The lights will be controlled synchronously.
I recommend you take a look at the JN-AN-1189-ZigBee-HA-Demo-1v15.pdf
Chapter: 6.2.2 Commissioning Light Nodes - Binding
Please follow the next path.C:\NXP\bstudio_nxp\workspace\JN-AN-1189-ZigBee-HA-Demo\Doc
Regards,
Mario