Hello,I use JN5168 made an application of tof,now I want to use JN5169,is JN5169 design with TOF?
Hi Yucheng Lin,
Unfortunately, the JN5169 doesn't provide a TOF module.
Reference to TIme of Flight in JN5169 DS has been removed.
Regards,
Mario
hi Mario
if the jn5169 doesn't provide a TOF module,is there any chip can repace jn5168?
our chip supplier said that jn5168 has been stop production
Hi Yucheng Lin,
We do not recommend this module, has a limited support and the measure, that you will get, won't be correct.
Mario
Hi Mario
If I use JN5168 as the TOF master,and use JN5169 as the TOF slave,is that correct?
Hi Yucheng Lin,
Unfortunately, we do not recommend using this module
Regards,
Mario
Hi Mario Ignacio Castaneda Lopez
but why I use the same progame with JN5168,it look like can work?
I use the TOF function in JN5169,the distance calculate by tof look right?