IW612 guard interval: What is the default setting?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IW612 guard interval: What is the default setting?

Jump to solution
480 Views
jun_1
Contributor III

What is the default guard interval for IW612? Is it fixed value or a dynamically variable value? I tried to check the details using mlanutl, but could not find the corresponding command.

0 Kudos
Reply
1 Solution
435 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @jun_1 

Thanks for creating case to us.

Let me check internally and feedback to you ASAP.

 

Best regards,

Christine.

View solution in original post

0 Kudos
Reply
4 Replies
417 Views
jun_1
Contributor III

Thank you for your reply.

0 Kudos
Reply
452 Views
jun_1
Contributor III

Let me give a supplementary explanation.

I'd like to know the default guard interval for 802.11n/802.11ac/802.11ax.

0 Kudos
Reply
427 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @jun_1 ,

 

See below, please!

-- For 802.11n/802.11ac, Guard Interval has 2 options:

(1) long GI : 800ns (0.8us) , it is also call 'normal' 

(2)short GI: 400ns (0.4us)

-- For 802.11 ax, Guard Interval has 3 options:

(1) long GI : 800ns (0.8us) , it is also call 'normal' 

(2)double: 1600ns (1.6us)

(3)quadruple: 3200ns (3.2us)

-- Using mlanutl to get or set Guard Interval

(1)Checking GI type

In README_MLAN document, you can see descriptions on if short GI or normal is enabled or disabled , no concrete time (period) of the GUI, because the correspond time has been fixed in 802.11 spec, like above. So you only need to check whether long GI or short GI, etc is enabled.

(2) For WiFi 6 setting

please refer to 'txratecfg'  session, definitions are like below:

For HE:
0 = 1xHELTF + GI0.8us
1 = 2xHELTF + GI0.8us
2 = 2xHELTF + GI1.6us
3 = 4xHELTF + GI0.8us if DCM = 1 and STBC = 1
4xHELTF + GI3.2us, otherwise.

 

So you can get default GI value when loading WiFi driver is done using mlanutl tool.

 

Thanks!

Regards,

weidong

 

 

0 Kudos
Reply
436 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @jun_1 

Thanks for creating case to us.

Let me check internally and feedback to you ASAP.

 

Best regards,

Christine.

0 Kudos
Reply