Hello,
What I am inquiring about is channel state information (CSI), and I am asking if there is a document or method to check the channel state around the AP.
For example, there seems to be a site that has an open source implementation of a util that extracts CSI from Broadcom chipsets.
Note: https://github.com/seemoo-lab/nexmon_csi
We ask if there is a way to extract CSI in a similar form for the NXP chipset.
Regards/I.S
Dear @isyu
Could you please confirm which driver and firmware versions you are using ? This is quite important, as the supported feature may depend on these versions.
Regards,
Olivier
Dear @ocourson
Kindly refer to the version information below
Wlan : SD-WLAN-SD-BT-8977-U16-MMC-W16.68.10.p237-16.26.10.p237-C4X16699_V2-GPL
(wlan: version = SD8977-68.16.237.p10-C4X16C699-GPL-(FP68))
Regards/I.S
Dear @ocourson
Please check the 88W8977 firstly if possible.
88W9098: PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p109.12-17.26.1.p109.12-MXM5X17312.P8_V0V1-GPL
Regards/I.S
Dear @isyu
88W8977 does not support CSI report
88W9098 FP68 release you are using support CSI.
Regards,
Olivier