Hello,
I want to flash new mac address in 88w8987. Using labtool I use the sequence:
2 => Use Bluetooth
Successful connect to hci1
45 => Read MAC from OTP
Get 41.41.41.41.41.41
46 aa.bb.cc.dd.ee.ff => Write MAC to OTP
Operation successfull
But after that the chip doesn't answer anymore to any labtool or hci command.
Spoofing the uart communication I get that:
< HCI Command: Read BD ADDR (0x04|0x0009) plen 0 #1 [hci0] 15.071800
> HCI Event: Command Complete (0x0e) plen 10 #2 [hci0] 15.074145
Read BD ADDR (0x04|0x0009) ncmd 1
Status: Success (0x00)
Address: 41:41:41:41:41:41 (OUI 41-41-41)
< HCI Command: Vendor (0x3f|0x0061) plen 32 #3 [hci0] 21.770553
00 00 01 04 37 0e 1c 00 ff ff ff ff 00 00 04 02 ....7...........
00 00 00 00 c0 c6 2d 00 ff ee dd cc bb aa f0 00 ......-.........
> HCI Event: Command Complete (0x0e) plen 4 #4 [hci0] 22.240375
Vendor (0x3f|0x0061) ncmd 1
Status: Success (0x00)
< HCI Command: Read BD ADDR (0x04|0x0009) plen 0 #5 [hci0] 26.152425
Bluetooth: hci0: command 0x1009 tx timeout
I'm using labtool 1.0.0.146
Can someone can explain why labtool fail ? Or give me an other way to sent mac address to the chip.
Thanks
Best,
Eric Delanghe
eric.delanghe@faurecia.com
Please give us some time, we are working on your request
Thanks
Hi,
Thank you Vincente. Do you know roughly, how much time it will take ?
Best
Sorry
we do not have a target day.
Regards
I just try the release 1.0.0.164 and it doesn't work. I link some new logs.
Do you know when an other release should be done ?