Does the inside of the RXD of TJA1043T have pull-up or pull-down applied?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the inside of the RXD of TJA1043T have pull-up or pull-down applied?

566 次查看
msjang
Contributor I

If not, can I pull-up with 10KR resistance external?

0 项奖励
回复
1 回复

559 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No, there is no internal pull-up or pull-down inside the RXD pin of the TJA1043T, pin RXD reflects the CAN Receiver value, if this is not happening, then an error is occurring.

Typically, this pin is directly connected to the uC without the need of an external pull-up.

 

If you are asking this because you need smooth the edges at bit transitions, I guess it would be better to use an up to 1 kΩ series resistor of on pin TXD.

 

Regards,

Jose Reyes

0 项奖励
回复