Battery life computation during BLE advertising

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Battery life computation during BLE advertising

Jump to solution
1,300 Views
danf
Contributor II

Using the 88W8977 BLE+Wifi chip I'm trying to understand how long the device can stay powered while advertising (as a BLE peripheral) using battery power.

In the datasheet there is a current consumption table which has:

Bluetooth LE advertise(interval=1.28s): 0.047mA @ 1.8V.

(With Wifi in deep sleep mode).

Is the value (0.047mA) the average current draw? so the battery life is simply:

Battery Life = Battery Capacity (mAH) / 0.047mA. (Assuming a 1.8V battery?).

example: Battery Life = 2500 mAH / 0.047mA --> 53,191 hours or 6.07 years

I understand this life is only accurate if the device does nothing else which isn't realistic, but I want to know if I understand the chart correctly.

Thanks!

 

0 Kudos
Reply
1 Solution
1,291 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @danf,

You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc. 

Regards,

Mario

View solution in original post

0 Kudos
Reply
2 Replies
1,287 Views
danf
Contributor II

Thanks! That makes sense. I appreciate your help!

0 Kudos
Reply
1,292 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @danf,

You are right it is the average in this scenario, but you have to be aware of the Current consumption during
device initialization, the modules that you will have enabled WIFI, etc. 

Regards,

Mario

0 Kudos
Reply