Based on i.MX8MN-EVK And Linux 5.4.70_2.3.0 BSP
As an example of NXP Bluetooth Bluetooth application, this article describes how to use Bluetooth to realize file transfer between windows PC and i.MX8MN-EVK (linux), and between Android mobile phone and i.MX8MN-EVK. The test architecture used in this example is as follows:
The following steps are for the application example:
Step 1 Preparation
--Downloading DEMO Image For i.MX8MN-EVK --Downloading uuu tool --Compiling L5.4.70_2.3.0 BSP for i.MX8MN-EVK --Copying rootfs to the DEMO Image directory --Modifying example_kernel_emmc.uuu as uuu programming script --Programming images to i.MX8MN-EVK board Booting i.MX8MN-EVK board
Step 2 Loading WIFI/BT driver and Enable Bluetooth Step 3 File Transter between Windows 10 PC and i.MX8MN-EVK board Step 4 File Transter between Android Mobile and i.MX8MN-EVK board [Summary]
More detailed information, see attachment, please!
記事全体を表示