I am using the VF5xx in a design for which the 1.5MB on-chip RAM is sufficient.
How should the DDR pins be connected in the design, given that they are unused?
So far I am assuming the following.
1. SDRAMC_VDD2P5 pins are connected to DECAP_V25_LDO_OUT.
2. SDRAMC_VDD1P5 pins are left floating
3. The following pins are connected to VSS:
DDR_A, DDR_D, DDR_BA, DDR_DQM, DDR_DQS, DDR_ODT, DDR_CAS,
DDR_CKE, DDR_CLK, DDR_CS, DDR_RAS, DDR_WE,
DDR_VREF, DDR_ZQ, DDR_RESET.
Is this correct?
Richard
已解决! 转到解答。
Hello Richard,
Sincerely, Naoum Gitnik.
Hello Richard,
Sincerely, Naoum Gitnik.
A) Rev 5 DS Figure 4 shows LDO2P5 supplying not just DDR but also several internal PLLs. Based on those extra connections, should the Tower capacitors on DECAP_V25_LDO_OUT be retained? (10u, 3x0.1u, 3x470p) Some LDOs are unstable without a certain minimum bulk capacitance on the output. It also seems like some decoupling (0.1u, 470p) might be helpful for keeping the noise level low for the sensitive PLL circuits?
B) Floating inputs make me nervous in general. Might it be better if we ground it? Do you see higher risk in grounding it as opposed to floating? I do see the note on page 31 regarding floating the supply but it doesn't state which (1P5, 2P5) it is referring to.
Thanks, Chris