In the timesys BSP User Guide BSP User Guide for Freescale TWR-VF65GS10 | Timesys Embedded Linux
Linux uses DMA channels on DMA engine 0,mux 0
UART1 RX - Channel 4
UART1 TX - Channel 5
DSPI0 RX - Channel 12
DSPI0 TX - Channel 13
SAI2 (I2S2) RX - Channel 20
SAI2 (I2S2) TX - Channel 21
But when i checked the in the linux # ls -1 /sys/class/dma
I can see that there are DMA assigned on DMA1:
dma1chan0
dma1chan1
dma1chan10
dma1chan11
dma1chan12
dma1chan13
dma1chan14
I would like to ask if it is possible to reroute DMA1 to DMA0?
I want to configure the Linux to only use DMA0 and the MQX to DMA1.
Hello Carlo,
Which kernel version is this in regards to? This is the same query in your ticket in our queue, correct?
Thank you,
Timesys Support
Hello timesyssupport,
In this test, i'm using the Kernel 3.1.13.
Hello Carlo,
Please find the attached patch, where Linux will no longer initialize DMA1. This modifies the vf610 device tree includes file, so all you need to do is apply this patch to your kernel sources, then rebuild your device tree blob for the hardware target (pcm052).
Thanks,
Timesys Support
timesyssupport please continue with the follow up.
timesyssupport can you help to attend this case?