Hi team,
Can user select 2pins as RMII_CLKOUTs at the same time and connect Ether PHYs with each pins?
If possible, what output delay time is there between each pins?
And, my understanding is the RMII_CLKOUT is PLL5 clk output signal. Is it correct?
Best Regards,
Hiroki
已解决! 转到解答。
Dear Hiroki,
Sincerely, Naoum Gitnik.
Dear Hiroki,
Sincerely, Naoum Gitnik.
Hi Naoum,
Mitsubishi is planning to produce an integrated control system of industrial air-conditioner. They want to use 2 ethernet devices concurrently. They connect Vybrid with 2 ethernet PHYs. So they confirm whethever Vybrid can provide RMII_CLKOUT to 2 external ethernet PHYs concurrently or not and then RMII_CLKOUT pins have delay or not.
And they are planning to use PLL5 as RMII clock source. Then does RMII_CLKOUT output PLL5 clock?
Best Regards,
Hiroki
Dear Hiroki,
Sincerely, Naoum Gitnik.