Videos testing out Freescale Cup kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Videos testing out Freescale Cup kit

Videos testing out Freescale Cup kit

Couple of new videos.

This time I am running the FRDM-TFC library demo code written by Eli Hughes without any change at all-- successfully on my car.

I have had the 0 ohm R24 res replaced with a higher one thanks to the soldering skills of David DiCarlo!

The first video highlights demo modes 0 through 3:

Car demos - YouTube

Demo 0- test buttons and switches

Demo 1- test servo

Demo 2- test motors

Second, I was able to get my little o-scope (xprotolab) to capture the camera analog out-- here:

Camera testing - YouTube

No major coding done but I understand the library and ports on the boards much better now.   Still haven't resolved the 'whining' apparent when I enable the H-bridge but I will try a few things this week-- it is possible it is harmless.

Next steps, buffering camera data then on to control loops!

Daniel

Oh, I was also able to get the serial port working while code was running so I could get some dynamic feedback.

This document was generated from the following discussion: Videos testing out Freescale Cup kit

标签 (1)
标记 (2)
评论

The "whining" you are hearing is the switching currents through the motor.    There is a macro in the code that sets the switching frequency of the PWM/H-Bridge Circuit.     I think the default tis 4KHz :-)

In my car I modulate in real-time to "hear" different stuff to debug the car....

无评分
版本历史
最后更新:
‎08-28-2013 12:29 PM
更新人: