T2080RDB Rev-C machine
In uboot, the NAND FLASH can be access using : nand dump 0 ... can printf some information
I run vxWorks OS in this RDB board, CPLD and NOR FLASH can work good, but NAND FLASH can not work good.
1、VxWorks OS version: 6.9
2、Initial IFC timing, and set the LAW values
3、NOR ---> CS0
CPLD ----> CS2
NAND ----> CS1
when i port the nand flash initial code to vxWorks, access the CS1 LAWs address space, i can not detect the CS1 singnal. and i found that when i just modify the NAND TIMING to work GPCM mode, CS1 falling edge singnal is present. why???? anybody can help me?
In case if you are observing CS1 is not asserted, when you accessing this address space, than this may mean:
1. CS1 address space is not configured.
2. LAWs are not configured.
3. Some other device is configured to overlap this address space.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------