deploy a boot image to a T2080 micro via CWTAP probe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

deploy a boot image to a T2080 micro via CWTAP probe

883件の閲覧回数
mrbe
Contributor II

Is it possible to deploy a binary image using ccs commands via a CWTAP probe?

ラベル(1)
5 返答(返信)

863件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @mrbe 

Could you please provide us with more information?

Which image would you like to deploy?

We will be aware for your kind reply.

BR,

Hector 

0 件の賞賛
返信

855件の閲覧回数
mrbe
Contributor II

Hi Héctor,

We are considering flashing the initialization binaries (RCW and boot binaries and so on) using the CWTAP and CCS commands as a manufacturing process. We wanted to create some kind of script to do it automatically as soon as the board is available from manufacturing. Our goal is to provide a manufacturing procedure to update the boot FW with minimal interaction from manufacturing operators, i.e. not allowing manufacturing operators to navigate CodeWarrior windows to download those binaries.

Could you help us to do that?

Thanks in advance.

M. Rosario Beltrán

 

0 件の賞賛
返信

826件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @mrbe 

Hope this post finds finds you well,

Yes, it is possible,

Please find attached on the case an application note in reference that can be useful for this situation.

"Bringing up Layerscape devices using CCS script and DRAM boot"

Have a great day.

0 件の賞賛
返信

787件の閲覧回数
mrbe
Contributor II

Hi Héctor,

Thank you very much for sending me this AN. To fully understand it to create my own script to initialize a T2080 board I would appreciate it you could send me a little explanation and how to handle the next list of ccs commands: 

ccs::config_template; ccs::config_chain; ccs::reset_to_debug; ccs::get_config_chain; ccs::run_core; ccs::stop_core; ccs::step_core; ccs::write_mem; ccs::read_mem; ccs::read_reg; ccs::write_reg; ccs::set_max_tck; ccs::core

If you prefer I ask for this by creating a ticket, please let me know

Thank you for all your help

 

776件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @mrbe 

We have a documentation that can be useful regarding your last reply.

Kindly create a new ticket and inform us that it is linked to case 00620959 by using the technical support web located in the following link:

https://support.nxp.com/s/

Best Regards,

Hector Villarruel

0 件の賞賛
返信