Dear NXP,
I am working on T4160RDB-64B machine. I want to know some of the image specification. I don't the importance of these images.
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
From this link (Table 110. NOR Flash Memory Map),
0xEFE00000 0xEFE3FFFF CORTINA PHY code (current bank) 256KB
0xE8700000 0xE87FFFFF HV.uImage (current bank) 1MB
0xE8900000 0xE89FFFFF HV config device tree (current bank) 1MB
0xE8A00000 0xE8CFFFFF Guest image #1 (current bank) 3MB
0xE8D00000 0xE8FFFFFF Guest image #2 (current bank) 3MB
0xE9000000 0xE92FFFFF Guest image #3 (current bank) 3MB
Please provide the necessity of these images.
May I want to flash these all images or these are the options ?
Should I flash these images ?
Thanks & Regards,
VInothS
CORTINA PHY code | PHY firmware. Required if the board has this PHY, unnecessary otherwise. |
HV.uImage, HV config device tree | NXP Hypervisor images. Required if you are working required in the basic Linux boot scenario. |
Guest image #1 - Guest image #3 | Hypervisor guest OS images. See above. |
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi bpe,
I am using e6500 rev2 core support and this is the virtual core to T4160RDB processor.
So, I will flash the NXP Hypervisor images also.
Is it right ?
Thanks & Regards,
VinothS
Yes, it is right
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you bpe for the quick response,
Thanks & Regards,
VinothS
Thank you Bpe,
I have e6500 rev2 core support also for this I want to flash HV.uImage, HV config device tree also.
Regards,
VinothS