T4240RDB new kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240RDB new kernel

644 Views
bogdantanasa
Contributor II

Hi,

I am trying to use a new configuration file for the kernel that comes with the freescale variant of yocto 1.6 for a t4240rdb board. I have performed the following steps:

1. bitbake -c menuconfig virtual/kernel

--- this allows me to create the .config file as I want.

2. In meta-fsl-ppc/recipes-kernel/linux I have created a file linux-qoriq-sdk_3.12.bbappend which contains

FILESEXTRAPATHS_prepend := "${THISDIR}/files:"

SRC_URI += "file://defconfig"

3. the .config create at 1. has been copied to meta-fsl-ppc/recipes-kernel/linux/files and renamed to defconfig

4. bitbake fsl-image-core

--- this builds everything. I assume that the new kernel will exactly be based on my defconfig file. Is this right?

As a result of 4 I see that in the work directory there is another directory named linux-qoriq-sdk/3.12-r0. There I can see my defconfig file. However, when I go to linux-qoriq-sdk/3.12-r0/image/usr/src/kernel there I see a .config file that is different from the defconfig file.

This means that the resulting kernel is built according to that .config file. (I assume so). If so, what am I doing wrongly?

Thanks,

Bogdan.

Labels (1)
0 Kudos
Reply
0 Replies