T2080 Regulator Query: LTC3877

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 Regulator Query: LTC3877

1,135 次查看
KLN
Contributor III

Hi Team,

We are using T2080 in one of our design.

Our total T2080 processor current calculation came around 24A. We are planning to use LTC3877 

VID Control regulator which is capable of 60A when Dual channel combined. 

Since our current is maximum of 24~25A, Can we use single channel of LTC3877 to make use of 30A of LTC3877.

 

In previous designs with T4241, Processor current of 56A, LTC3877 Dual Channel combined Output (60A Capable Dual channel combined) was used.

 

Please confirm, In our case Single channel of LTC3877 can be used?

Thanks.

4 回复数

1,106 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello KLN

Hope this post finds you well,

Yes, it can be used as long as you supply the necessary current consumption.

BR,

Hector Villarruel

0 项奖励
回复

1,101 次查看
KLN
Contributor III

Hi @Hector_Villarruel 

Thanks for your reply. It's not clear.

What do you suggest us using Single channel LTC3877 (30A) or Dual Channel?

As previously said, Current consumption of core(max) is 24~25A.

Can we go ahead with single channel?30A?

0 项奖励
回复

1,084 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello KLN,

Regarding to your question:

Can we go ahead with single channel?30A?

Yes, you can go ahead as long as you supply the necessary current consumption using a single channel.

BR,

Hector

 

0 项奖励
回复

1,119 次查看
KLN
Contributor III

Hi Team, 

Awaiting for your response.