T1042 Uboot config for x32 DDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 Uboot config for x32 DDR4

1,008 Views
gokulkrishnan
Contributor III

Hi, 

If I am intending on using a x32 configuration for the flash. What are the changes or implications that may come up while loading the uboot. can you help me with that? Also if there are changes that I need to make in the configuration please let me know.

Regards

Gokul

Labels (1)
0 Kudos
Reply
5 Replies

836 Views
Bulat
NXP Employee
NXP Employee

I am not sure what "changes" you are asking about? If you mean changes between x64 and x32 DDR interfaces, you need to properly set DDR bus width via DDR_DDR_SDRAM_CFG[DBW] register, and correct memory size (assuming the same x64 memory is used in x32 mode).

Regards,

Bulat

0 Kudos
Reply

836 Views
gokulkrishnan
Contributor III

Hi,

By changes I meant the settings that I must look into. So just the DBW needs to be set right?

Regards 

Gokul

0 Kudos
Reply

836 Views
Bulat
NXP Employee
NXP Employee

Yes.

0 Kudos
Reply

836 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, you said "I am intending on using a x32 configuration for the flash", but topic name says "x32 DDR4"

Can you clarify this discrepancy between "flash" and "DDR4"?

0 Kudos
Reply

836 Views
gokulkrishnan
Contributor III

Hi Alex, 

Sorry My bad got mixed up. i meant DDR itself.

0 Kudos
Reply