IBIS (DDR4) and IBIS-AMI Model for T1042

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IBIS (DDR4) and IBIS-AMI Model for T1042

795 Views
gokulkrishnan
Contributor III

Hi, 

Could you please provide the  IBIS (DDR4) and IBIS-AMI Model for T1042 chip for simulation purpose?

Also could you provide the S-Parameter models for the package.

The part number we are using is the following: T1042NSE7WQB.

Also it would be great if you could provide any supporting documents for the above mentioned items.

Regards 

Gokul

Labels (1)
0 Kudos
Reply
1 Reply

606 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Unfortunately, the processor's IBIS-AMI model is not public. Please open technical case to obtain additional information:

How I could create a Service Request?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply