I have a custom board with T1042 and component DDR4 in 64 bit interface.
I am using the Codewarrior TAP tool to try and bring up DDR4, but When I try, I get following error:
"Error configuring the target! - DDR initialization failed: D_INIT was not cleared by hardware!"
Is there a list of things the T1042 does to attempt this? What exactly does this mean?
Trevor
Please check whether there is problem with the DDR controller initial configuration parameters.
If there is SPD on the target board, please use reading from SPD to create a DDR project.
If no, please create a QCVS DDR project with default parameters, then modify Properties panel according to DDR datasheet.
Would you please capture the low level CCS log to me to do more investigation?
When connecting CodeWarrior to your target board, CodeWarrior Connection Server(CCS) will pop up in the Windows task bar. Please open CodeWarrior Connection Sever console, type "log v", then connect to the target board again, the low level CCS log will be printed in CCS console, would you please capture the CCS log and attach it here?
Discussing with the AE team.
is this a new board design? or an existing board design that customer has changed the DIMM part number?
if this is a new board bring up then:
please provide:
1. customer schematics (DDR section) for review.
2. how many board has customer tested and how many fail?
3. check all the DDR voltages and clocks, and send scope shots
4. put DRAM reset signal and HRESET signal on the scope and trigger on the rising edge of the HRESET signal. zoom out sufficiently to be able to capture the assertion and de-assertion of both HRESET and DRAM reset signals. when scope is setup, run a functional test on CW and provide the captured scope shot.
the expectation is that the DRAM reset signal will follow the same/similar assertion and de-assertion of HRESET signal.
change the following register
DQ_map0 0x00000000
DQ_map1 0x00000000
DQ_map2 0x00000014
DQ_map3 0x94000000
if it still fails, then run a WRC test in QCVS then after failure via ccs collect the DDR register log.
How to get register dump via ccs
This is for debug use only.
1) Open a CCS window (C:\Freescale\CW4NET_xxxxxx\Common\CCS\bin\ccs.exe)
2) Physical connection: USB to PC, JTAG to the customer board.
3) SW connection: in the ccs window type:
delete all
config cc cwtap
ccs::config_chain t1040
display ccs::read_mem 0 0x30000 0x8000 4 2 1024
ccs::write_mem 0 0x30000 0x8FB0 4 2 0x10000000
display ccs::read_mem 0 0x30000 0x8000 4 2 1024
Hi, Yiping
I have an update for you. After setting those registers as you suggest, most of the Codewarrior DDR4 validation items are passing.
There is one that is not, though. The "BIST-Write-then-Read-No-Turnaround" test is consistently failing while all the others are consistently passing. What is the difference between the No-Turnaround test and the others?
Also, we are trying to understand what the registers you sent are doing (below), can you clarify?
DQ_map0 0x00000000
DQ_map1 0x00000000
DQ_map2 0x00000014
DQ_map3 0x94000000
Trevor
the BIST no turnaround is not working in the tool. the failures are because of the tool and the an actual failure of the DDR interface. recommendation is not use the BIST with no turnaround.
the DQ_MAPn registers, provide the mapping information of the DRAM DQ order to the controller. controller uses this information during the initialization when training pattern are send and received. when controller does not have or has the wrong map it is not able to perform initialization of DRAM chips.
Will discuss with the AE team.
Hi Yiping,
Thank you very much for the recommendations.
I am currently working on performing this test, and will respond soon with detailed results. Initial results are encouraging.
Trevor
Hi Yiping
I did as you asked. the log is below
(bin) 1 % log v
CCS Windows Release Build 439p0
verbose logging
CCSAPI connection #1 accepted from ITE03005703.northgrum.com at Wed Mar 20 08:29:02 2024
check_min_version(serverh=0,*version)
api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
connections: {0,73,0xa9fecc5d}
cc_version(serverh=0,cc_index=0,index=0,*version)
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
devlist: t10xx
reset_to_debug(serverh=0,cc=0)
available_connections(serverh=0,*count,*cc)
connections: {0,73,0xa9fecc5d}
get_config_chain(serverh=0,cc=0)
*** unhandled(command=163) ***
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C00,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C04,size=4,space=0},count=4,*data)
data: 80000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C08,size=4,space=0},count=4,*data)
data: 81000013
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C10,size=4,space=0},count=4,*data)
data: 00000001
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C14,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00000C18,size=4,space=0},count=4,*data)
data: 81000020
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008000,size=4,space=0},count=4,*data)
data: 010002FF
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008008,size=4,space=0},count=4,*data)
data: 0300033F
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008010,size=4,space=0},count=4,*data)
data: 0340037F
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008018,size=4,space=0},count=4,*data)
data: 038003BF
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008080,size=4,space=0},count=4,*data)
data: 80010212
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008084,size=4,space=0},count=4,*data)
data: 00000202
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008088,size=4,space=0},count=4,*data)
data: 00000202
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000808C,size=4,space=0},count=4,*data)
data: 00010202
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000080C0,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000080C4,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000080C8,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000080CC,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008100,size=4,space=0},count=4,*data)
data: 01161000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008104,size=4,space=0},count=4,*data)
data: 4055000C
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008108,size=4,space=0},count=4,*data)
data: CCCA0E54
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000810C,size=4,space=0},count=4,*data)
data: 0049111C
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008110,size=4,space=0},count=4,*data)
data: 65200000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=4,space=0},count=4,*data)
data: 00401050
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008118,size=4,space=0},count=4,*data)
data: 01010225
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000811C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008120,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008124,size=4,space=0},count=4,*data)
data: 18600618
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008128,size=4,space=0},count=4,*data)
data: DEADBEEF
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008130,size=4,space=0},count=4,*data)
data: 02000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008148,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000814C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008160,size=4,space=0},count=4,*data)
data: 00220001
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008164,size=4,space=0},count=4,*data)
data: 07401400
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008168,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000816C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008170,size=4,space=0},count=4,*data)
data: 8A090705
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008174,size=4,space=0},count=4,*data)
data: 8675F605
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000817C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008180,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008184,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008190,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008194,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000081A0,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000081A4,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000081A8,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000081AC,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008200,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008204,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008208,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000820C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008210,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008214,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008220,size=4,space=0},count=4,*data)
data: 00000900
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008224,size=4,space=0},count=4,*data)
data: 04000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008228,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000822C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008230,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008234,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008238,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000823C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008250,size=4,space=0},count=4,*data)
data: 05115800
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008260,size=4,space=0},count=4,*data)
data: 00002000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x000082A0,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008400,size=4,space=0},count=4,*data)
data: 5B65B658
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008404,size=4,space=0},count=4,*data)
data: D96D96D8
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008408,size=4,space=0},count=4,*data)
data: 5B65B658
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x0000840C,size=4,space=0},count=4,*data)
data: D96D8000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008B20,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008B24,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008B28,size=4,space=0},count=4,*data)
data: 80040000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008B2C,size=4,space=0},count=4,*data)
data: 0000A181
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008BF8,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008BFC,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D00,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D20,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D24,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D28,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D2C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D30,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D34,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D38,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D3C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D40,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D44,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D60,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D64,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D68,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008D6C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E00,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E04,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E08,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E20,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E24,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E28,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E40,size=4,space=0},count=4,*data)
data: 8000119D
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E44,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E48,size=4,space=0},count=4,*data)
data: 0000001D
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E4C,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E50,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E54,size=4,space=0},count=4,*data)
data: 00000000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E58,size=4,space=0},count=4,*data)
data: 00010000
write_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008110,size=4,space=0},count=4,*data)
data: E5200000
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008114,size=1,space=0},count=4,*data)
data: 00 40 10 50
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E20,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E24,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E28,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E40,size=1,space=0},count=4,*data)
data: 00 00 00 80
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E44,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E48,size=1,space=0},count=4,*data)
data: 00 00 00 1D
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E4C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E50,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E54,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008E58,size=1,space=0},count=4,*data)
data: 00 01 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F00,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F04,size=1,space=0},count=4,*data)
data: 00 00 30 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F08,size=1,space=0},count=4,*data)
data: 00 00 00 0C
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F0C,size=1,space=0},count=4,*data)
data: 14 00 0C 20
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F10,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F14,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F18,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F1C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F20,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F24,size=1,space=0},count=4,*data)
data: 10 10 10 10
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F28,size=1,space=0},count=4,*data)
data: 10 10 10 10
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F2C,size=1,space=0},count=4,*data)
data: 10 10 10 10
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F30,size=1,space=0},count=4,*data)
data: 10 10 10 10
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F34,size=1,space=0},count=4,*data)
data: 10 10 30 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F38,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F3C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F40,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F44,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F48,size=1,space=0},count=4,*data)
data: 00 00 00 01
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F4C,size=1,space=0},count=4,*data)
data: 11 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F50,size=1,space=0},count=4,*data)
data: 0E 00 0D 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F54,size=1,space=0},count=4,*data)
data: 0F 00 0F 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F58,size=1,space=0},count=4,*data)
data: 10 00 10 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F5C,size=1,space=0},count=4,*data)
data: 11 00 12 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F60,size=1,space=0},count=4,*data)
data: 11 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F64,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F68,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F6C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F70,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F74,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F78,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F7C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F80,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F84,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F88,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F8C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F90,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F94,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F98,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008F9C,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FA0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FA4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FA8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FAC,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FB0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FB4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FB8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FBC,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FC0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FC4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FC8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FCC,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FD0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FD4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FD8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FDC,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FE0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FE4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FE8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FEC,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FF0,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FF4,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FF8,size=1,space=0},count=4,*data)
data: 00 00 00 00
read_memory(coreh.{serverh=0,cc_index=0,chain_pos=0},
addr.{addr_hi=0x00030000,addr_lo=0x00008FFC,size=1,space=0},count=4,*data)
data: 00 00 0C 00
CCSAPI connection #1 from ITE03005703.northgrum.com closed at Wed Mar 20 08:29:30 2024