SD Card not detected by T4240QDS u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD Card not detected by T4240QDS u-boot

Jump to solution
2,821 Views
aloishahn
Contributor III

Hi,

 

could anybody give me a hint about how to use the SD Card Slot on the T4240-QDS?

I want to setup my system for SD Card deloyment. I did a similiar thing on T4240RDB and T2080RDB already, which works fine there.

 

Now, on the T4240QDS, my SD Card is not detected by u-boot.

I would expect to see the SD Card in u-boot with command "mmcinfo".

Actually it lists an mmc, but it seems to list the internal MMC only, but the external is not visible.

 

=> mmcinfo

Device: FSL_SDHC

Manufacturer ID: fe

OEM: 14e

Name: MMC04

Tran Speed: 52000000

Rd Block Len: 512

MMC version 4.0

High Capacity: Yes

Capacity: 3.6 GiB

Bus Width: 4-bit

=> help mmc

 

mmc list does not show the external SD Card, just the internal on, independent of either the external us plugged in or not

=> mmc list

FSL_SDHC: 0

=>

 

For reference I have attached the whole boot log "t4240qds-boot.txt"

 

Any ideas?

 

best regards

Alois

Original Attachment has been moved to: t4240qds-boot.txt.zip

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,184 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 2.11.1 of the T4240QDS Reference Manual. It looks like that SDHC_CD and SDHC_WP ara assigned to I2C using cfg_mux_i2c3 configuration signal.

View solution in original post

0 Kudos
Reply
2 Replies
2,185 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 2.11.1 of the T4240QDS Reference Manual. It looks like that SDHC_CD and SDHC_WP ara assigned to I2C using cfg_mux_i2c3 configuration signal.

0 Kudos
Reply
2,184 Views
aloishahn
Contributor III

Hi Pavel,

works fine now, found SW7[4]=ON to switch from internal to external SD.

many thanks ans best regards

Alois

0 Kudos
Reply