Missing base address of CPC Partitioning Control Registers in user documentation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing base address of CPC Partitioning Control Registers in user documentation

ソリューションへジャンプ
1,779件の閲覧回数
nakrachi
Contributor II

Hi Everyone,

As part of the platform cache flushing procedure, the T1042 RM states that "Clear all bits in CPCPAR0-CPCPAR15 " but we couldn;t find the base address of CPCPAR in the reference manual.

nakrachi_2-1634136827775.png

it looks like it was removed :

nakrachi_0-1634136492182.png

I know (using the Trace32) that the base address for CPC_PAR0 is CROSSBAR_ADR+0x10208, but we need to confirm this with NXP to document it as a rational.

thank you

0 件の賞賛
返信
1 解決策
1,774件の閲覧回数
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

元の投稿で解決策を見る

2 返答(返信)
1,775件の閲覧回数
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

CPC_CPCPAR0 address is equal to:

base address (specified by the CCSRBAR) + 0x1_0000 (CPC block offset address) + 0x208

1,768件の閲覧回数
nakrachi
Contributor II

Thank you

タグ(1)
0 件の賞賛
返信