Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

Jump to solution
1,415 Views
Larry5335
Contributor IV

Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,173 Views
Bulat
NXP Employee
NXP Employee

I am not sure if it has been varified, however it should be ok with 16GB DIMM.

I think "larger" size is not applicable to the T2080RDB, main restriction is the number of ranks. iI maximum it supports dual-rank SODIMM, or in other words only two CS's are connected to the SODIMM socket and 16GB is the maximum size.

Regards,

Bulat

View solution in original post

0 Kudos
Reply
1 Reply
1,174 Views
Bulat
NXP Employee
NXP Employee

I am not sure if it has been varified, however it should be ok with 16GB DIMM.

I think "larger" size is not applicable to the T2080RDB, main restriction is the number of ranks. iI maximum it supports dual-rank SODIMM, or in other words only two CS's are connected to the SODIMM socket and 16GB is the maximum size.

Regards,

Bulat

0 Kudos
Reply