I have download Codewarrior10.6 Evaluation version and save the license.dat in C:\fresscalse\CW for MCU10.6\MCU, but when in use mwcceppc.exe in cmd, will aslo report no valid license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have download Codewarrior10.6 Evaluation version and save the license.dat in C:\fresscalse\CW for MCU10.6\MCU, but when in use mwcceppc.exe in cmd, will aslo report no valid license

1,129件の閲覧回数
dabizi
Contributor I

I have download Codewarrior10.6 Evaluation version and save the license.dat in C:\fresscalse\CW for MCU10.6\MCU, but when in use mwcceppc.exe in cmd, will aslo report no valid license.

 

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>mwcceppc.exe -c aa.c

### mwcceppc.exe Driver Error:

#   License check failed: No such feature exists.

#   Feature:       Win32_Plugins_Comp_PPC

#   License path:  C:\Freescale\CW MCU v10.6\MCU\license.dat;

#   FLEXnet Licensing error:-5,357

#   For further information, refer to the FLEXnet Licensing documentation,

#   available at "www.macrovision.com".

 

 

please help me...

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

832件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please check whether you have set the PATH Environment Variable in the script when building with command line tools:

SET CWFolder= C:\Freescale\CW MCU v10.6.4\MCU

SET LM_LICENSE_FILE=%CWFolder%/license.dat

Hope this helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

832件の閲覧回数
dabizi
Contributor I

Hello Fiona :

Thanks for your repley!

I have set the Environment Variable in my .bat file (Codewarrior10.6, the license.dat was obtained from NXP evaluation):

SET PATH=C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools;

SET CWFolder= C:\Freescale\CW MCU v10.6\MCU

SET LM_LICENSE_FILE=%CWFolder%\license.dat

SET MWCIncludes=C:\Freescale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_C\include;C:\Freescale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_Runtime\Runtime_PA\Include;

SET MWCLibraries=C:\Freescale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_C\include;C:\Freescale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_Runtime\Runtime_PA\Include;

mwcceppc.exe -char unsigned -c C:\LDRA_Toolsuite\CodeWarrior\MPC56xx\__ppc_eabi_init.c

pause

The result is :

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>SET PATH=C:\Freescale\

CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools;

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>SET CWFolder= C:\Frees

cale\CW MCU v10.6\MCU

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>SET LM_LICENSE_FILE= C

:\Freescale\CW MCU v10.6\MCU\license.dat

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>SET MWCIncludes=C:\Fre

escale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_C\include;C:\Freescale\CW MCU v10.6\M

CU\PA_Support\ewl\EWL_Runtime\Runtime_PA\Include;

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>SET MWCLibraries=C:\Fr

eescale\CW MCU v10.6\MCU\PA_Support\ewl\EWL_C\include;C:\Freescale\CW MCU v10.6\

MCU\PA_Support\ewl\EWL_Runtime\Runtime_PA\Include;

C:\Freescale\CW MCU v10.6\MCU\PA_Tools\Command_Line_Tools>mwcceppc.exe -char uns

igned -c C:\LDRA_Toolsuite\CodeWarrior\MPC56xx\__ppc_eabi_init.c

### mwcceppc.exe Driver Error:

#   License check failed: No such feature exists.

#   Feature:       Win32_Plugins_Comp_PPC

#   License path:   C:\Freescale\CW MCU v10.6\MCU\license.dat;C:\Freescale\CW

#   MCU v10.6\MCU\Bin\..\license.dat;

#   FLEXnet Licensing error:-5,357

#   For further information, refer to the FLEXnet Licensing documentation,

#   available at "www.macrovision.com".

That is to say SET LM_LICENSE_FILE does not work.

Please help me if there is anthor way to resolve this problem.

0 件の賞賛
返信