Can i able to extend the evaluation licence period?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i able to extend the evaluation licence period?

10,463 Views
sheelahariharan
Contributor I

Hi,

 

Im using codewarrior 5.1 and evaluation licence expires on April 1st. Is it possible to extend this licence till may 31st?

Labels (1)
0 Kudos
Reply
12 Replies

9,908 Views
trytohelp
NXP Employee
NXP Employee

Hi Shella,

There is a process to extend the evaluation period.

Please refer to the post:

    How to extend my evaluation license file for CodeWarrior

If you meet a problem to get it you can also contact the license team via the Case system.

Refer to the post:

    How to log an issue in Case system instead CRM (Service request - not used anymore)?


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,908 Views
sheelahariharan
Contributor I

HI,

I tried to extend the license period as per the post mentioned. But on doing that im getting the following error even with the old license file. Pls suggest how to proceed.

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply

9,908 Views
trytohelp
NXP Employee
NXP Employee

Hello Sheela,

It seems the key for IDE is missing or wrong.

To solve the problem I recommend you to edit your license file and add the following lines:

+++++++++++++++++++++++++++++++++++++

FEATURE Win32_CWIDE_Limited metrowks 5.5 permanent uncounted \

    00E825C5615A HOSTID=ANY TS_OK

#

##################################################################

####  CW HC12 v5.1 license

##################################################################

#

INCREMENT Win32_CWIDE_Unlimited metrowks 5.900 permanent uncounted \

    C10A4505A261 VENDOR_STRING="CodeWarrior IDE 4.2 or later, \

    Windows" HOSTID=ANY ck=134 TS_OK

INCREMENT ProcessorExpertHCS12 metrowks 1.001 permanent uncounted \

    3DBC1127AF17 VENDOR_STRING="Basic \

    beans;1880BA310687F4EDA26BE3E59EB4D4E0" HOSTID=ANY ck=64 TS_OK

+++++++++++++++++++++++++++++++++++++

This is the standard special Edition license file.

If you will still have a problem, you should have the keys for:

    Win32_CWIDE_Limited

    Win32_CWIDE_Unlimited

      ProcessorExpertHCS12

Remove the keys and keep these ones only


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,908 Views
sheelahariharan
Contributor I

Hello Pascal,

I’m not able to find the keys in my license.dat file.

I have attached the license file. Can you please tell me where to copy the keys?

My win OS is win7-64 bit.

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply

9,908 Views
trytohelp
NXP Employee
NXP Employee

Hi Sheela,

In all case this license can not be used.

The keys have expired since 16-mar-2016.

For me you're not using the right license file.

In our web license system I've found your evaluation registration under your account.

The Expiration Date is defined to 04/01/2016 (Expiration Date: Apr 1, 2016).

I've downloaded the new temp license and corrected the keys just to be sure it will work fine.

Attached the new file - rename it to license.dat.

Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,908 Views
sheelahariharan
Contributor I

Hello Pascal,

I didn’t find any attachment in the mail. Can you please resend me..

Also is it possible to extend the license date till 31st march in the same file?

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply

9,908 Views
trytohelp
NXP Employee
NXP Employee

I see the attachment.

You need to open the "full" post:

     Can i able to extend the evaluation licence period?

The file is out.txt.zip.

Pascal

0 Kudos
Reply

9,907 Views
sheelahariharan
Contributor I

Hi Pascal,

I have downloaded and replaced the license file into the specific path.

Then also I’m getting the following error, pls help

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply

9,907 Views
trytohelp
NXP Employee
NXP Employee

Hi,

You should not have this error as the Unlimited key is included in the license file.

Now I know in some case this could arrive.

I added the Limited Key too.

Please use the attached license file.

Pascal

0 Kudos
Reply

9,906 Views
sheelahariharan
Contributor I

Hello Pascal,

Still im facing the same issue.

Are there any other ways to make it work?

I tried reinstalling the setup files again but still this license issue persists.

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply

9,907 Views
trytohelp
NXP Employee
NXP Employee

Hi Sheela,

The license file sent is running fine.

This license is not locked on any PC and it's running fine on my side with HC12 V5.x.

I think there is a problem under your PC.

Are you sure you're using the right license file ?

I recommend you to perform a search on all locals Hard drives for license.dat and rename the file to license .dat_ for instance.

At the end when you will try to launch the IDE you should get an error saying no license file was found.

Flexlm should return an error code -1.

pastedImage_2.png

At this point any license file was found.

You can check if you've an environment variable LM_LICENSE_FILE and remove it in case of.

Then you can add the license file I sent in the main installation folder.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,911 Views
sheelahariharan
Contributor I

Hello Pascal,

Thanks for the help. I renamed all the license file I had in my laptop and reinstalled the codewarrior again.

Its working fine.. Thankyou ☺

Thanks and Regards,

Sheela Hariharan.

Electronics - IVN & Diagnostics

0 Kudos
Reply