question about FMEDA of 33771&33772

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about FMEDA of 33771&33772

575 Views
Chenlong_Wu
NXP Employee
NXP Employee

Regarding the FMEDA of 33771&33772, I have a question on OCs ASIL level.

before information is that with/without use SM39(Use of AN5 and AN6 as Current Measurement input), the ASIL level of OC shall be C and B.

but I found in each FMEDA, 771B/771C/772B will change from D to B when disable SM39

772C will change from D to C when disable SM39

Do you know why 772C can reach ASIL C without use SM39?

And if our FMEDA consider external filter circuit?

0 Kudos
Reply
4 Replies

541 Views
SavinoLupo
NXP Employee
NXP Employee

Hi Chenlong Wu,

thank you for the excellent question.

It took me time to check. I saw the customization of the MC33771C calculation has a problem like the one found in the MC33772C Excel file, which was corrected. I attach the new version of the work MC33771C FMEDA, which will be uploaded to nxp.com. You will see the issue is solved, the result after the customization is ASIL C.

Regards,

Savino

0 Kudos
Reply

516 Views
Chenlong_Wu
NXP Employee
NXP Employee

Hello @SavinoLupo 

got the information of 33771C, and thank you for your quickly answer.

How about the B version?

In my opinion, there are no different between B version and C version on Current function.

if B version still only meet ASIL B without SM39,  and why?

thanks!

Chenlong

0 Kudos
Reply

539 Views
SavinoLupo
NXP Employee
NXP Employee

However, keep in mind that the FMEDA result is at IC level, it gives no guarantee that ASIL C is met at system level, because the absence of the double filter will not allow to easily detect failure modes on the filter sitting on the PCB.

0 Kudos
Reply

561 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

I have asked our BMS Safety Expert and author of the Safety Manual/FMEDA to answer this question.

BRs, Tomas

0 Kudos
Reply