mm9z1_638 current accuracy is out of 1% requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mm9z1_638 current accuracy is out of 1% requirement

1,158 Views
a852013777
Contributor III

Hi Nxp partner 

After we perform AN12301 calibration guide, we record the current reading from mm9z1_638. We found there are 3 to 5 reading is over our accuracy 1% requirement. Do you have any Low pass filter from software or hardware? How to determine the low pass cofficient?Do you reference guideline?

a852013777_1-1681716380417.png

 

a852013777_0-1681715601735.png

 

 

0 Kudos
Reply
2 Replies

1,149 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mike,

Looking at the data, it seems there is some periodic lower reading, where is this coming from? Is this from the test equipment or SW?

Capture.JPG.png

Seems this periodic event is causing the issue.

Best regards,

Tomas

0 Kudos
Reply

1,126 Views
a852013777
Contributor III

Hi Tomas

 

Thanks, we chagne another electrical current source. the fail condition was fixed.

but we performed the 6A accuradcy can't meet +/-1%, The noise is about  100mA . Do you have suggestion reduce the 100mA noise ? or the 100mA noise is acceptable.

a852013777_0-1681982767855.png

 

Br,

Mike  Liang

 

0 Kudos
Reply